Radar 77Ghz

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,552件の閲覧回数
josephharden
Contributor I

I am a part of a team of students at the University of South Carolina and we are hoping to design a mobile radar application for the university (range of at least 100m). We've looked at 77Ghz modules that are available. Do you have any suggestions on where to start or what we can use?

I'm hoping we can use the modules shown in the video below. (Qorivva MPC577xK MCU and the MRD3000 multi-channel 77 GHz radar transceiver chipset)

77GHz Radar Automotive Safety System - YouTube

We need to obtain the variables that he mentioned in the video and process them using logic. Are there any educational materials available or places to start?

Starting from scratch is a bit daunting. :smileyconfused:

Thanks,

Joseph

ラベル(1)
1 解決策
3,845件の閲覧回数
josephharden
Contributor I

Thank you so much,

I'll be sure to contact her. Thanks again for the help!  :smileyhappy:

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,845件の閲覧回数
FlavioStiffan
NXP Employee
NXP Employee

dear Joseph

there is no didactic material for the 77GHz radar suite at this point. I would recommend getting in touch with Damaris Ochoa who is managing the Americas relationships with universitieS. She might be able to put you in touch with a professor locally that can help getting you started.

3,846件の閲覧回数
josephharden
Contributor I

Thank you so much,

I'll be sure to contact her. Thanks again for the help!  :smileyhappy:

0 件の賞賛
返信