University Programs Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

University Programs Knowledge Base

Discussions

Sort by:
We are excited to be coming to Rice University to tell you about Freescale.  Please RSVP and join us at our informational session and career expo. If you'd like to pre-submit resumes please do so here! javierprado - (LinkedIn) - Digital Networking - Design Manager at Freescale Jonathan Burnett - (LinkedIn) - Signal Intregrity Norman Herr Cheryl Lednicky Andrew Mawer James Vacek Charles Calvin greghale - (LinkedIn) -  Engineer noahllozada Ben Schmid Jason Nearing Maureen Helm - (LinkedIn) Mark Lohman - (LinkedIn) - Design Lead
View full article
El proyecto se trata de un tiro al blanco que funciona con una pistola que emite luz infrarroja, la cual es captada por los sensores infrarrojos localizados en el centro de los blancos. De atinarle al blanco, este se esconderá y aparecerá uno nuevo.
View full article
Added by Joe Grand on June 21, 2012
View full article
15. Juli 2011, Audi Training Center am Flughafen München: Der eb011 absolviert den ersten Testrun. Brake Test erfolgreich, die ersten Runden wurden gedreht. ...
View full article
Qorivva Based Freescale Cup Webinars:  Lecture 1: Introduction and Motor Basics Lecture 2: Pulse Width Modulation Lecture 3: Control Design Lecture 4: Speed and Position Lecture 5: MPC5607B Overview
View full article
Characteristics of This Book (1) General knowledge and relevant knowledge are well-balanced. From the standpoint of application, this book explains the general principles of the embedded system’s “general knowledge” in a concise but logically lucid way; at the same time, it also pays attention to the coherence between the general knowledge and relevant knowledge about chips. So with the understanding of general principles, the reader can better understand chip application design, which in turn contributes to the understanding of the former. (2) Both hardware and software design are a concern. An embedded system is the efficient integration of hardware and software. So its design should be a design with coordinated, rather than completely separated, hardware and software, like that of a general computer. It is especially true for intellectual embedded application in electronic systems that embedded software cannot be developed well without considering the hardware, and vice versa. (3) Component-based packages of low level drivers are provided. Every module in the book has been furnished with a driver program (in line with the basic principles of the embedded software project and the requirement of a component-based package), detailed, with standard notes and an interface. The supply of low-level driver components for practical application facilitates transplantation and reusability, which saves the reader time for developing his project. (4) Advisable test examples are supplied. Every source program listed in the book has been tested. All test cases are reserved in this book’s CD to free the reader from the trouble caused by design fault or the innate mistake of these example routines, and to facilitate the reader’s confirmation and comprehension. (5) The CD provides all low-level drivers’ component package procedure, texts and test cases. When used, it also contains a chip reference manual, installation and usage about the writing device, tool software (for example, development environment, program writing and reading software, serial ports adjusting tools, USB device, as well as Ethernet tools), related hardware schematic, other technical information, etc. (6) Hardware evaluation, writing adjusting device, and software tools that can solely conduct program writing and reading are supplied to facilitate the reader to practice and apply. Contents There are altogether 16 chapters in this book. The first chapter is an introduction to knowledge system, learning mistakes and learning suggestions on embedded systems. The second and the third chapter describes the characteristics of the ColdFire MCU family, gives the pin function of MCF52233 and the minimum system circuit as well as the first sample program and ColdFire project system to complete the introduction to the first ColdFire project. Chapters 4-10 deal separately with UART, Keyboard,LED and LCD, A/D, Timer,QSPI, I2C and online programming of Flash Memory. And from the eleventh chapter to the fifteenth chapter, information concerning CAN Bus of MCF52235, Ethernet modeling on MCF52233, other modules of MCF52233, USB 2.0 programming of MCF52233, the transplantation and application of μC/OS-Ⅱin ColdFire are provided. The last chapter gives an account of developing methods of embedded systems based on hardware component. Appendix A lists the chip packaging of the ColdFire MCU family used in this book. Complete course files restricted to verified faculty only.  Available for download in the Faculty-Portal
View full article
2013 Global Freescale Cup Participant Video Link : 1588 Car Specs: FRDM-K20D50M
View full article
Discussion of how to setup interrupts on the NVIC. The Flex timer is used as an example
View full article
Our first testing on an university track. The track was very slippery so the robot had big problems to keep the line. Traveling around 1-2m/s
View full article
MathWorks is a proud global sponsor of The NXP Cup If you are a member of a NXP Cup team, you have access to a complimentary Software License for MATLAB / Simulink. Visit the NXP Cup - MathWorks Deutschland website to learn more about the Software offering.  Examples for using Simulink in the NXP Cup are packaged with the Simulink Coder Support Package for  FRDM-KL25Z available from the Hardware Support Page.  Additional examples for reading and analyzing live data from the Line Scan Camera are available in the NXP Cup Companion App available on the MATLAB File Exchange.  Additionally, there is an example which uses the Simulink Coder product from MathWorks to target the FRDM-KL25Z. Feel free to use the forum on MATLAB Answers or here below to ask your questions about MATLAB use with The NXP Cup.  You can also email [email protected] with any questions.
View full article
Freescale india and CEDT, IISc organised Smart car race india 2010 winner team from NIT,Surat. Students: Maulik Gandhi , Rikil Shah and Samir Sirohi.
View full article
Team Wooden Jalopy from the University of Applied Sciences in Landshut on their run at the Freescale Cup Europe Finals in Prague (2012-04-04). We ranked the 5th place.
View full article
FTF on-the-street reporter talks to the Universidad del Valle de Mexico team from Guadalajara, Mexico who describe their challenge...
View full article
The first step of starting your TFC project is to get to know your microcontroller. This article serves you as an introduction of Qorivva MPC560xB microcontroller. Qorivva MPC5604B Summary The Qorivva MPC560xB/C/D family of 32-bit microcontrollers (MCUs) includes the latest in integrated devices for automotive electronics applications. These scalable Power Architecture® devices are supported by an enablement ecosystem that includes software drivers, operating systems and configuration code to help you quickly implement your designs.  For the Freescale Cup Challenge, we have provided Tutorials, example code and projects which are based on the trk-mpc5604b StarterTRAK evaluation board. Which Chip do you have? The chipset mounted on the boards for the Freescale Cup can vary. Always validate your chipset to know it's full capabilities. MPC560xB Product Information Page Difference's At-a-Glance: 5604B = 512MB Flash; no DMA 5606B = 1MB Flash; Has 16-Channel DMA 5607B = 1.5Mb Flash; Has 16-Channel DMA Getting Started Presentation Getting Started with MPC5600B.pptx (2Mb) Important Resources: e200z0 Core Reference Manual TRK-MPC5604B User's Manual TRK-MPC5604BQuick Reference Guide TRK-MPC5604B Schematics Reference manual Freescale's Qorivva MPC560xB Page Power.Org
View full article
Lab Materials that accompany the LFEBS12UB. Download restricted to verified faculty only.  Request to join the Faculty Portal now.
View full article
El hombre a través de la historia ha buscado comunicarse de manera eficaz con sus congéneres. Ha desarrollado diversos aparatos que facilitan dicha acción, desde el teléfono, que permite escuchar la voz de otro humano rompiendo las barreras de la distancia y el tiempo. Pero desafortunadamente los mayores esfuerzos se focalizan en las mayorías y los estándares de un hombre común. Esta aplicación nos dará la oportunidad de comunicarnos de una manera más fácil con las personas que no pueden hacerlo mediante el habla. Mediante circuitos instalados en la mano, compuestos por un material que podrá hacer sentir al operador más libre. Estarán hechos con tinta conductiva amigable, esto quiere decir que no daña la salud del operador. En base a cerrar circuitos y sensores de proximidad hechos con la tinta con relación a la posición de los dedos con base en el alfabeto dactilológico se reproducirá una palabra a través de una bocina que el operador portara consigo para que el usuario pueda escuchar una traducción de la composición del mencionado alfabeto. #include "mbed.h" #include "MMA8451Q.h" #define MMA8451_I2C_ADDRESS (0x1d<<1) DigitalIn dedo1(); DigitalIn dedo2(); DigitalIn dedo3(); DigitalIn dedo4(); AnalogIn flex_dedo1(); AnalogIn flex_dedo2(); AnalogIn flex_dedo3(); AnalogIn flex_dedo4(); AnalogIn dedos unidos(); DigitalIn puno1(); DigitalIn puno2(); /* Aqui ira una funcion en la cual se relaciona todas las entradas anteriores y se les da un valor en el alfabeto, ya sea palabra, oracion o frase.*/ int main(void) {     MMA8451Q acc(PTE25, PTE24, MMA8451_I2C_ADDRESS); //el programa correra en un ciclo, que leera cualquier movimiento de los dedos y lo almacenara y a su vez lo relacionara con la funcion correspondiente hasta que el usuario baje su mano //por el momento solo imprimira en una pantalla ya que el programa que estuve usando para la generacion de palabras me diante la comunicacion serial de la targeta a la pc tiene dueño, buscare desarrollar mi propia aplicaion. }
View full article
Overview Please check your local rules to confirm allowable voltage, battery chemistry and ampere-hour as these differ by region. This article is NOT a substitute for the rules. Batteries (nor Charger) are not included in the Freescale Cup kit due to global shipping complexities. Batteries can be hazardous if not stored, used and/or disposed of properly. Battery Specifications Tamiya Connector 7.2 Volts Less than or equal to 3000mAh (Check your Rules!) NiCd or NiMH Needs to have a Tamyia connector Sources of purchase   This format battery is fairly common in the radio controlled toy industry. Start your search at any local electronics store where Radio controlled toy's are sold. Retail Sources: Radio Shack (USA) - http://www.radioshack.com/product/index.jsp?productId=4273066 Fry's (USA) - http://www.frys.com/product/6468002?site=sr:SEARCH:MAIN_RSLT_PG   Online Sources All-Battery.com http://www.all-battery.com/nicd72v2400mahhighpowerbatterypackforrccarswithtamiyaconnector.aspx http://www.all-battery.com/Tenergy7.2V3000mAhRCCarNiMHBatteryPackwithCharger-91103.aspx Europe: use Conrad online stores Conrad energy NiMH Sub-C Racingpack 7.2 V / 2400 mAh Stecksystem Tamiya-Stecker im Conrad Online Shop | 206026 (Conrad Germany but same available form other sources)
View full article