University Programs Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

University Programs Knowledge Base

Discussions

Sort by:
Model provided by the Mathworks Academic support team to manage wide angle lenses on the default Freescale Cup car camera.
View full article
O Protótipo deste Robô foi desenvolvido com base em algumas informações do projeto Robô Curiosity da Nasa. O presente protótipo captura imagens por uma câmera wirelles e o sistema Labview tratará estas imagens. Possui comunicação RF e USB. Outras informações estão contidas no anexo.
View full article
Tested race, TUSUR, Tomsk, Russia 😃
View full article
     El juguete consiste en 3 botones de un tamaño adecuado. Cada uno precederá a una tira o serie de leds. El programa ejecutará una instrucción que creará una secuencia de valores aleatorios, los cuales, por así decirlo, descenderán por las tiras de leds. El niño tendrá que presionar los botones en el tiempo en el que la luz alcanza y permanece en el botón. Muy similar al videojuego Guitar Hero. El aumento de dificultad es mediante el aumento de la rapidez de juego; será regulada según la posición de un potenciómetro. También será posible decidir el número de botones a usar.      El modo de uso no se limita a las manos, podrá ser usado con los pies sin problema alguno. Para hacer eso posible cada botón será independiente de los otros dos, lo que permitirá el acomodo más ergonómico de los botones según las limitaciones de movilidad del niño. Para evitar el desplazamiento de los botones por la superficie: suelo, alguna mesa... los botones se fijarán a un tapete de Velcro.
View full article
Instructions There are several main hardware configuration steps. Once the USB cable has been connected between the evaluation board and PC, it may be necessary to update the chip firmware which requires moving a jumper pin on the evaluation board. Then, connect one end of the USB cable to the PC and the other end to the Power/OSJTAG mini-B connector on the TWRK60N512 module. Allow the PC to automatically configure the USB drivers if needed. Before updating the firmware, it is necessary to start a CodeWarrior Project. In this case, the easiest way to do this is to actually navigate to the sample project and click on the Sample.mcp file. This will open CodeWarior 2.8. Selection Project->Build Configurations->MK40X256VMD100_INTERNAL_FLASH Project-»Build All Run->Debug Configurations—> Use the Codewarrior download Filter and Select "PROJECTNAME_MK40XD256VMD100_INTERNAL_FLASH_PnE_OSJTAG" Additional step is required if the firmware is out of date: Firmware Upgrade Instructions (if needed)   Firmware may change after an evaluation board has been manufactured and shipped. As a result, an alert will be displayed during the first attempt to download software to the board. Follow the instructions carefully. 1.     Unplug the USB cable.   2.     Look for the jumper (On the REV B Board) labeled "OSBDM_IRQ" - it is jumper 35. It will be found between the on/off switch and to the right of the the white "Lin" connectors. Remove one of the "LED Enable" jumpers for this if you don't have a   header jumper handy and put the jumper on the OSBDM_IRQ header These LED Jumpers are just above the blue potentiometer knob and marked as "J27."   3.    Reconnect the USB cable and click OK.   4.     Wait for the new firmware to download. 5.     A new dialog will appear when the process is complete.  6.    Unplug the cable, remove the jumper, return it to the location it was "borrowed from" and reconnect the cable. 7.    Then click OK.
View full article
There are several programs on the market which are freely available. Below is a list of the more popular [free] ones.  Eagle PCB 123
View full article
El presente proyecto busca solucionar de una manera práctica y divertida actividades de terapia que pueden ser parte de la vida de cada persona con necesidades especiales, especialmente infantes. Por medio de este proyecto se pretende desarrollar la memoria y el orden lógico. Utilizando un sensor óptico para la lectura de pequeños Cubos de colores, el carro donde será transportado el sensor óptico emitirá una nota musical, misma que dependerá del color del cubo. El equipo de trabajo está conformado por cuatro   estudiantes del Tecnologíco de M
View full article
Hi,     I will present to you my first personal initiated project named Spectrum analyzer. This spectrum is based on sampling signal and calculating his spectrum using FFT algorithm. Attached here presentation, documentation (french), electrical scheme of amplification circuit and source code of both programs (Computer and PXS20)   Picture of the spectrum analyzer with TWR-PXS20, TWR-SER and TWR-PROTO :   Picture of amplification circuit :   Picture of signal collected by the ADC :   And here we have the spectrum :   Thank you, and I hope you like it
View full article
This document is addressed to the participants and visitors that will join us for The Freescale Cup 2015 Worldwide Finals 2015 The Freescale Cup 2015 Worldwide Finals will be held on 14-15 September 2015 at the Fraunhofer Institute for Integrated Circuits (Fraunhofer IIS) in Erlangen, Germany. Full address is: Fraunhofer IIS Am Wolfsmantel 33 91058 Erlangen Germany Google Maps location The attendees official guide is now online at https://community.nxp.com/docs/DOC-106164 Agenda of the event for the participants (subject to change): Sunday September 13th: Arrival at Hotels Get together in the evening (approximate time 18:00) at A&O Hostel Monday September 14th: 8:30: Departure from Hotel for City Tour 11:30: Prepare for departure for Fraunhofer IIS 12:00: Buses depart for Fraunhofer IIS 13:00: Lunch 14:00: Opening session 15:00: Start of Practice 17:30: High School and Innovation Challenge Demos 18:00: End of Practice - Start of the evening event 21:00: End of evening event - boarding buses for return to hotel Tuesday September 15th: 8:00: Buses depart for Fraunhofer IIS 9:00: Practice 13:00: Technical Inspection & Lunch 14:30: Final Race 16:00: Awards Ceremony 17:30: Buses depart for Awards Dinner 20:30: Buses depart for Hotel The event will be presented via LiveCast by the Fraunhofer IIS. URL is http://www2.iis.fraunhofer.de/freescale/  Hotel information: Students Hotel: Nuremberg Hostel - Stay at the A&O Hostel & Hotel Nuremberg  Google Maps Location Professors and Press Hotel: NH Nürnberg City Center hotel in Nuremberg Bahnhofstr. 17-19 | NH Hotel Group Google Maps Location Freescale will cover the cost of travel, accommodation and meals for the event for all Freescale Cup qualified teams and one faculty advisor per the rules in place. For Visa invitation letters, please contact [email protected] or [email protected] Travel booking will be organized by your regional Freescale University Program contact. Please have your faculty advisor get in touch with them for more information
View full article
Pulse-width modulation (PWM), is a technique utilized in robotics for controlling motors and servos. Through the use of internal counters, the microcontroller modulates the duty cycle of a square wave to control the amount of power delivered to a device. The Duty Cycle referes to the porportion of time the square wave is 'on' as compared to the repeating signal period. The higher the duty cycle the higher the power carried in the signal. Duty cycle is expressed as a percentage of time the signal is 'on', with 100% being consistently on.  overview-create-a-pwm-signal Once you feel comfortable that you understand the concepts behind a duty cycle signal, return to Reference Manual: Timer Information portion of the Drive A DC Motor Tutorial
View full article
Official rules of the Global Freescale Cup! New in 2014 - Roll-out of leagues: Depending on region there will now be three leagues.  The Global race will only be stock league vehicles. Stock League - Racing using approved components, less customization allowed Custom League - Racing with less restrictions and custom hardware Innovation League - More than just racing.  Complete an objective or task to score points and win. Notes You can view this document in PDF format using the Action Menu bar. This rule set is for the Worldwide challenge.  Find your regional rules here The Worldwide challenge is only open to the stock (unmodified) challengers at this time. If you have ANY questions about these rules, post them in the comments section below.  If you have questions about regional rules, ask in your regional group. Section 1: Team Requirements A regional championship team must run a “stock” (unmodified) league to qualify. Four person maximum team size. A team may have only one graduate student. Cars will be designed and constructed by students ONLY.  Participants, advisers, and audience are expected to exhibit good sportsmanship. Any inappropriate behavior or cheating may result in disqualification. Section 2: Event Registration Entrants into the worldwide challenge are by invitation only. One invitation is extended to each regional champion team. One person from the regional champion team must register the entire team for the worldwide challenge within two weeks after the conclusion of the regional final.  Section 3: Equipment Requirements Each team shall use the same basic kit of parts as described below.  The following requirements are in place to keep the playing field level.  You must use one of the approved controller and motor driver boards.  If any standard component of the car model is damaged, then the same replacement component should be used. Mechanical The original and unaltered equipment must be used in the entry.  Outer tire treads and rim Drive - DC motors Transmission Ratio of Drive Motor Servo Motor Allowed modifications and restrictions: You may not change the wheel base (distance between wheels) No part of the car shall exceed dimensions of 250mm/9.85in (W) x 400mm/15.75in (L)x 305mm/12in.(H) You may drill holes and mount auxiliary pieces on the chassis assuming it is contained within the above dimensions. You may change the orientation of the servo motor and related linkages. You may add a "skin" to the car but it must be removable during inspection. You may adjust or remove springs, linkages, and other non-essential pieces. You may adhere the tread to the rim.   Electrical Battery (purchase separately) 7.2V, <=3000mAh, rechargeable NiCd or NiMH  Only one (1) battery at a time may be used to power the vehicle and any attached hardware You must use one of the approved boards below to control your car. Control System FRDM- series of boards The FRDM-KL25Z is included but not mandatory to use. TRK- series Kinetis based TWR- series High Voltage Motor Control and Interface TFC-SHIELD The TFC-SHIELD is included but not mandatory to use. The Dual Motor Control Board from Landzo technologies. Allowed modifications and restrictions: One processor - No auxiliary processor or other programmable device is allowed.  The car must use a optical sensor to navigate DC-DC boost circuit may not exceed battery voltage. Total capacity of all capacitors should not exceed 2000 uF. Sensor Limits You may use additional cameras.  Maximum of sixteen (16) sensors Examples of sensor count:  IR Transmitter/Receiver pair is 1 sensor A CCD sensor is 1 sensor The provided Line Scan Camera is 1 sensor A hall effect sensor on two rear wheels is 2 sensors An encoder mounted on one wheel is 1 sensor A display (is allowed) does not count as a sensor Section 4: Vehicle Inspection Before the race, the judges will perform a technical inspection of all entries. This includes vehicle specifications, dimensions, and equipment requirements listed in Section 3. All cars must be placed in the Inspection area on or before the designated time. Once in the Inspection Area, you may not touch car until you are called to race! In the event of any violations, the organizing committee may disqualify the corresponding team. Section 5: Timed Race Procedure Race order will be determined by a random drawing. When your team is called you may remove your car  from inspection area.  You will have two (2) minutes to prepare the car. Approved Adjustments - You may: Configure parameters via on-board interfaces. (Switches, Knobs, etc.) Alter the angle of your camera Change batteries  Disallowed Adjustments -You may not: Reprogram your processor Configure parameters via wired or wireless communications. There shall be only one team member on the track at any given time. (excludes testing times) Before the 2 minute expires you must signal “Ready” to the referee before starting car. After the referee confirms “Ready”, the vehicle should leave the starting area within 30 seconds. Teams have THREE attempts to complete ONE lap.  The FIRST (not the best) completed time will be recorded. Example: Attempt 1 – Vehicle goes to fast around a curve and goes off track.  Time is not recorded. Attempt 2 – Vehicle makes it around track successfully.  Time is recorded. Attempt 3 – Is forfeit because FIRST time (Attempt 2) has been recorded. After each attempt you have two minutes to make approved (see above) adjustments to vehicle. After the attempts, the team shall return the vehicle to inspection area. Event displays will post the times after each team races. Section 6: Race Day Schedule Practice Time - Prior to final race, a test track will be available. Final calibration may be made at this time.  This will be organized with team slots and/or “free-time”.   2. Reconfigure practice track to final track. Vehicle Inspection (see section 4) Timed Race Awards Ceremony Section 7: Event Personnel Organizing committee – A committee of senior judges and Freescale event organizers.  Will coordinate event day activities and mediate and resolve any disputes. Referees -  Responsible for on-track activities. This includes race track management such as starting and stopping vehicles, as well as timing and scorekeeping. Comprise up of of faculty, student, and/or Freescale and industry employees. Judges  - Interpret and enforce rule compliance.  This will be comprised of Freescale employees and members of contributing industry sponsors. Event Personnel shall not aid any one specific team. Communication shall be open to all teams and shall not disclose any information that might compromise the fairness of the competition. Section 8: Fouls, Failure and Disqualifications The rules will be interpreted by Freescale and the organizing committee of the event.             Foul, is a minor infraction, which results in time penalties. Failure, results in the current attempt time not being recorded. Subsequent attempts are allowed. Disqualification is a major infraction which results all times not being recorded. Referee will determine whether the racing car ran out of the race track and assign time penalties. Any of the following conditions will be considered a foul and will result in time penalty added: The race car fails to leave the starting area within 30 seconds after beginning of the race [+1 second]. The race car fails to stop 2 meters/6 feet or leaves the track after crossing the finish line [+1 second]. Any of the following conditions will be considered a failure and no time will be given: Three or more wheels leave the race surface. The racing team fails to get prepared for the attempt within the two (2) minutes allotment. The player touches the race car after the technical inspection without consent of the referee. The race car fails to finish within 120 seconds after leaving the starting area. Touching the car at any time between start and finish. "Start" - Once the vehicle crosses the starting line. "Finish" - Once the vehicle crosses the finish line. Any of the following conditions will be considered a disqualification:   Any off track equipment or behavior that may influence or impede cars.   Doing a Disallowed Modification anytime after Inspection. More than one team member in the playing field. Any cheating during the competition. Failure to pass the technical inspection. Equality and fairness will be ensured as much as possible on the condition of actual feasibility.  Disputes will be resolved by a vote of Freescale, members of the organizing committee, and judges. Section 9: Timing/Scoring Time will be captured using an electronic gate and/or handheld timer. Time starts and ends when the first part of the racing car breaks the start/finish line. Fouls will result in the time addition to the car’s lap time. Disqualifications and Failures will result in no score. Section 10: Parameters of the Racing Track A test track made from the same material as the final track will be made available on the day prior to the final race for calibration and design modifications. The actual layout of the final racing track will be unknown to competitors until competition day. Width of the racing track shall not be less than 600mm/23.65in. Material and dimensional specifications can be found on the community. Surface of the racing track is matte white, with a continuous black line (25mm/1in wide) on each edge of the track. The racing track can intersect with a crossing angle of 90°. The racing track can have inclines, declines,  and tunnels. The rules and conditions are subject to change by Freescale if necessary. Freescale reserves the right in their sole discretion to cancel, suspend and/or modify The Freescale Cup race at any time. These official rules are drawn up in the English language. If these official rules are provided in any other language and there is a conflict in the text, the English language text shall prevail. Freescale and the Freescale logo are trademarks or registered trademarks of Freescale Semiconductor, Inc. in the U.S. and other countries. All other product or service names are the property of their respective owners. © Freescale Semiconductor, Inc. 2014
View full article
Many companies run the risk of animals such as rats and variety of insects invading plants or warehouses, where the products are liable to be contaminated, mainly food industry companies. For the above, we come up with the development of the “pest control using Freescale” which consists of implementing an electronic device that emits ultrasonic frequencies ranging from 30KHz to 65KHz generated by the FRDM KL25Z board transmitted by a buzzer and through an interface may change the operation time of our prototype. Therefore purpose of this project is to solve the pest problem in a "green way" to avoid damaging the environment. Original Attachment has been moved to: Pest_control_using_Freescale.rar
View full article
La descripción de este proyecto consta principalmente de tres elementos que destacan el primero y el cual es tomado como planta principal es un reloj despertador el cual esta conformado por un freedom, un LCD de 16x2 caract. y por una pequeña bocina, este será controlado para su funcionamiento con el módulo touch del micro-controlador; como segundo apartado se tiene una tira de LEDS que se empotra a la cabecera de la cama la cual contendrá un dimmer para controlar la cantidad de luz, teniendo como máxima intensidad la hora fijada en la alarma (como apoyo además de la bocina para lograr despertar) y por último un interruptor de apagado que se pretende colocar al otro lado de la habitación donde se desee incorporar el despertador, el cual tendrá forma de canasta de baloncesto, para que solamente al anotar una canasta sea la única forma de apagar la alarma y este proceso sea interactivo. Original Attachment has been moved to: fcup.zip
View full article
http//www.freescale.com/UniversityPrograms -- Students from the University of Science and Technology in Beijing share the challenges and teamwork that went i...
View full article
Tested race, TUSUR, Tomsk, Russia 😃
View full article
Recommend accessories or post your own designs.  For the community by the community! Add your contributions in the comments section below.  As I filter through them I will move them up into this main document, so it is easier to browse. TFC Camera Mounts Designed by Wave Number Print these on demand via Shapeways.com Base Board Hinge Two Position Tower Elevator TWR-ELEV-2 — Wavenumber LLC - Link to the Store
View full article
Project Summary In this project, you will learn how to do basic electrical automation and control via the web.  Think of the NEST.... only more open and hackable!   Using Websockets, Javascipt and HTML5,  you will have a simple way of viewing remote data and be able to control some solid state relays.   This framework will allow you to create more complex IoT applications.    The example will combine a FRDM-K64F and a FRDM-AUTO to read a temperature sensor and control a solid state relay. Skills Developed: Embedded Systems Networking Electrical Control Systems HTML5/Javascript - Websockets SOIC8 and 1206 Surface mount soldering Internet of "Things" Materials: FRDM-K64F FRDM-AUTO Development Tools mbed.org Google Chrome Notepad++ Example Code mbed.org Github Step 0: Prerequisite Videos The videos are organized into a nice YouTube playlist: FRDM-AUTO Hardware Overview MonkeyDo Software Overview Websockets & The MonkeyDo communication model Solid state relay introduction & sage Opto-coupler introduction & usage MonkeyDo system demonstration Step 1: Get a FRDM-AUTO & FRDM-K64 The build package is on the FRDM-AUTO site.   Note that for this exercise you only need to build the "OPTION 1" version.  Please let us know if you are interested in a pre-assembled version.  If there is enough demand we will get a lot assembled for purchase, I will get a Kickstarter going!   Don't be afraid to build it yourself,  Soldering is fun!  There is plenty of good stuff on the web on how to do SMT soldering.  All of the parts on the board are fairly simply once you get the hang of it and everything can be hand soldered  The key is having some decent tools. Step 2: Put it Together Assemble the FRDM-AUTO and K64F.   When you get started, do NOT hook up anything to the solid state relays until you are sure  things are working. WARNING:   Wiring to household power can be dangerous!   You are 100% responsible for what you do. Be careful and never apply power until you fundamentally understand what you are wiring up! Step 3: Download If you have never used the mbed environment,   make sure to careful read this page.   Get the "blinky" programming working before you try anything else. Download the example firmware to the FRDM-K64F.    Make sure to press the reset button. Step 4: Follow Along Make sure to watch the demo video.   Load the example javascript pages from the github repo and recreate what you see in the demo video.   Note:   You should NOT use the websocket server used in the demo code.     When you register for an mbed account, you automatically get your own websocket server channel. See Websocket server by Mbed. Step 5: Hack and Slash! Make something cool!   Be cool and publish your work! Some Ideas to Extend the System Get the opto-couplers into the Websocket system and see if you can report their state Make a basic thermostat using the temperature sensor and relay to control a heater. Report status via the websockets interface  
View full article
Feel free to print or post this poster on your bulletin boards to promote the registrations for The Freescale Cup EMEA 2016!! Should you need customisation for your school or university, please contact me
View full article
FreescaleCup race test - Team 3,14 STU Bratislava Slovakia 31.3.2012 High Speed Camera 400fps
View full article