ユニバーシティ・プログラムのナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

University Programs Knowledge Base

ディスカッション

ソート順:
Congratulations to all the teams to making it this far.  Last minute tweaks made and broke a few teams shooting for the top spot. Best times: (in seconds) 14.89 - Beijing University of Science and Technology [China] 17.60 - Swinburne University of Technology [Malaysia] 19.08 - National Taiwan University of Science and Technology [Taiwan] 19.57 - Escola Politecnica da Universidade de Sao Paulo [Brazil] 20.54 - University of California Berkeley [USA] 22.14 - Slovak University of Technology [Slovakia] DNF - The University of Tokyo [Japan] DNF - Bannari Amman Institute of Technology [India] DNF - Instituto Politecnico Nacional [Mexico] Read more: Day 1: Freescale Cup 2013 Worldwide Championship and China Regional Finals Day 2:  (coming soon)
記事全体を表示
Congratulations to all teams of the inaugural West Coast Freescale Cup event!  Our three fastest times, covering a total distance of 147 feet.  Full collection of event photos and videos!! Top 3 Teams: * First Place - UC Berkeley - 21.27 seconds Second Place - UC Davis - 27.92 seconds Third Place -  UC Davis - 28.00 seconds
記事全体を表示
Congratulations to all the East Coast teams and to UC-Berkeley for the overall fastest car in the USA!  More photos/videos from the event. West vs. East Winner: Jolt - UC-Berekley 17:35 East Coast Teams: First Place: Relativistic Robotic Racers - University of Rhode Island - 22.04 seconds Second Place: Vulcar - California University of Pennsylvania - 25.15 seconds Third Place: Temple Made - Temple University - 25.72 seconds See complete results
記事全体を表示
Instructions There are several main hardware configuration steps. Once the USB cable has been connected between the evaluation board and PC, it may be necessary to update the chip firmware which requires moving a jumper pin on the evaluation board. Then, connect one end of the USB cable to the PC and the other end to the Power/OSJTAG mini-B connector on the TWRK60N512 module. Allow the PC to automatically configure the USB drivers if needed. Before updating the firmware, it is necessary to start a CodeWarrior Project. In this case, the easiest way to do this is to actually navigate to the sample project and click on the Sample.mcp file. This will open CodeWarior 2.8. Selection Project->Build Configurations->MK40X256VMD100_INTERNAL_FLASH Project-»Build All Run->Debug Configurations—> Use the Codewarrior download Filter and Select "PROJECTNAME_MK40XD256VMD100_INTERNAL_FLASH_PnE_OSJTAG" Additional step is required if the firmware is out of date: Firmware Upgrade Instructions (if needed)   Firmware may change after an evaluation board has been manufactured and shipped. As a result, an alert will be displayed during the first attempt to download software to the board. Follow the instructions carefully. 1.     Unplug the USB cable.   2.     Look for the jumper (On the REV B Board) labeled "OSBDM_IRQ" - it is jumper 35. It will be found between the on/off switch and to the right of the the white "Lin" connectors. Remove one of the "LED Enable" jumpers for this if you don't have a   header jumper handy and put the jumper on the OSBDM_IRQ header These LED Jumpers are just above the blue potentiometer knob and marked as "J27."   3.    Reconnect the USB cable and click OK.   4.     Wait for the new firmware to download. 5.     A new dialog will appear when the process is complete.  6.    Unplug the cable, remove the jumper, return it to the location it was "borrowed from" and reconnect the cable. 7.    Then click OK.
記事全体を表示
Recommend accessories or post your own designs.  For the community by the community! Add your contributions in the comments section below.  As I filter through them I will move them up into this main document, so it is easier to browse. TFC Camera Mounts Designed by Wave Number Print these on demand via Shapeways.com Base Board Hinge Two Position Tower Elevator TWR-ELEV-2 — Wavenumber LLC - Link to the Store
記事全体を表示
WARNING If you stumble across the "getting started page" FREEDOM BOARD / CORTEX M0+ GETTING STARTED Please take note: While working with a large number of Freedom boards in a course,  it was observed that the Init Clock Routines would *sometimes* not work.    *Some* of the crystals on the freedom boards do NOT like "HIGH_GAIN" mode.   change the line   pll_init(8000000, HIGH_GAIN, CRYSTAL, 4, 24, MCGOUT); to   pll_init(8000000, LOW_POWER, CRYSTAL, 4, 24, MCGOUT);
記事全体を表示
Further Reading MCU 101: How does a DC Motor work? MCU 101: Pulse Width Modulation for DC Motors Specifications of Included DC Motor Conditions of Standard Operation Driving Voltage: 7.2V Direction of Rotation: CW viewing from metal housing Position of Motor: Horizontal Operating Temperature: 10 to 30 (Celsius) Operating Humidity: 30%RH to 95%RH Electrical Characteristics No Load Speed: 16000+/- 3200 rpm No Load Current 220mA (max) Mechanical Noise (Distance from housing side A=10cm Background Noise =30dB (max) 75 dB Stall Current: (two points method 1.2&3.9mNm) 3800mA (max) Stall Torque (two points method 1.2&3.9mNm) 80g.cm min End Play of Shaft 0.05~0.60 mm
記事全体を表示
The Freescale Cup East China 2013 challenge video 2 After formal competition finished in East China, we gave a challenge and asked teams to try a hill with >30 angle, some cars successes
記事全体を表示
Examines the core used in the MKL25Z128VLK4 device that is mounted on the FRDM-KL25Z board. The audience will be guided through the process of acquiring documentation for both the device and the core. A brief overview of the ARM cortex series will be presentated and how it relates to the embedded systems landscape.
記事全体を表示
Video Highlights of 2012 Competition Photographs from the Freescale Cup Japan 2012 competition.
記事全体を表示
1.  Go to community.freescale.com and Log in with your www.Freescale.com account, if you don´t have one, create one. 2.  Create a New Document 3.  Write your Project Name and a paragraph with a quick description of your project. Next, click the insert video icon to add your video of your project working. 4.  If your Project Report is less than 3 pages long, post it right below the video. If not, add it as Attachment. 5.  Also add your complete program project in a .zip file as an attachment. 6.  In the Category section, select if is a Student Project or other. 7.  In the Tags section, add any search words that can help anyone to find your project. Use University_Programs, your evaluation board name (ex. TWR-K40X256-KIT) and family (ex. Kinetis ). It is optional if you want to add your_university_name, region (ex. latin_america, emea), etc. 8.  In the Collaboration Options, add your team members if you want them to be able to edit it. And set Comments to be "Open". 9. Select Publish when you are done.
記事全体を表示
Photos Videos
記事全体を表示
Congratulations to the winning teams!! First Place Second Place Third Place Mach Pi- Universidade de Sao Paulo Poli - Gryphon- Universidade de Sao Paulo Zohan- Universidade do Estado de Santa Catarina Final Time: 15.52 Final Time: 18.27 Final Time: 20.1 David Nissimoff Diego Negrao Coordinator: Vitor Nascimento William Ricardo Kishimoto Diniz Jéssica Barbosa Heluany Wesley Wein Chen Coordinator: Fuad Kassab Junior Jean Ribeiro Fernandes Marcus Vieira Soares Rodolfo Lauro Weinert Coordinator: Ana Watanabe *Download zip file for more pictures.
記事全体を表示
A simple demo code for TWR-K60D100
記事全体を表示
Instructions There are several main hardware configuration steps. After installing the battery, once the USB cable has been connected between the evaluation board and PC, it may be necessary to update the chip firmware which requires moving a jumper pin on the evaluation board. Install the included battery into the VBAT (RTC) battery holder. Then, connect one end of the USB cable to the PC and the other end to the Power/OSJTAG mini-B connector on the TWRK40x256 module. Allow the PC to automatically configure the USB drivers if needed. Before updating the firmware, it is necessary to start a CodeWarrior Project. Open Codewarrior Navigate to File-> New ->Bareboard Project Select Kinetis K40->MK40X256VMD100 , P&E Open Source Jtag, C Language, No Rapid Application Development ,Finish Click on the main.c To get project focus Selection Project->Build Configurations->MK40X256VMD100_INTERNAL_FLASH Project-»Build All Run->Debug Configurations—> Use the Codewarrior download Filter and Select "PROJECTNAME_MK40XD256VMD100_INTERNAL_FLASH_PnE_OSJTAG" Additional step is required if the firmware is out of date: Firmware Upgrade Instructions (if needed) Firmware may change after an evaluation board has been manufactured and shipped. As a result, an alert will be displayed during the first attempt to download software to the board. Follow the instructions carefully. Unplug the USB cable. Look for the two pins labeled JM60 Boot and put a jumper on those pins Note: As it comes from the factory, the K40 board has a free jumper on the board. . Jumper J13 is labeled "JM60 BOOT." It connects two header pins which set the evaluation board in the firmware programming mode. This jumper is behind the LCD screen, and right next to LED/Touch Sensor "E3". Remove the LCD creen to gain access to the jumper. Reconnect the USB cable and click OK. Wait for the new firmware to download. A new dialog will appear when the process is complete. Unplug the cable, remove the jumper, and reconnect the cable. Then click OK. (You can store the jumper on the board, just set it so that it does not connect pins.) You may or may not encounter the firmware issue, or the multiple configurations issue. Once resolved, you should not see them again. With propertly set up hardware, users can return to Step 3: Import the LED Project of the Blink a LED on Kinetis Tutorial
記事全体を表示
prueba con una linea recta y una ligera curva a maxima velocidad
記事全体を表示
Continuing with the "warp drive controller example", this video explains low level hardware interfacing via bit manipulation. An example programming sequence for the warp drive will be shown. View Video Link : 1455
記事全体を表示
Harvard Extension School CSCI E-251, Fall 2012: Principles of Operating Systems Final Project Presentations Introduction by Prof. James L. Frankel
記事全体を表示
In this video we will discuss clock distribution in the KL25Z device. An example of initializing the PLL with the on-board crystal will be demonstrated.
記事全体を表示
Check out my website for more: www.nicopinkowski.com
記事全体を表示