技术日 - 培训资料

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Technology Days - Training Material

Training Sessions Material



Home

Home is where the heart is..

Home Control & Security; Development Software & Tools

Automotive

Automotive

讨论

排序依据:
Sensors are key to differentiate your products in the market and add context awareness, tamper detection, a robust user interface and accurate media compatibility. This class will step through some of key the leading applications in the Medical and Industrial markets that have found usage of motion and pressure sensors as well as some up and coming applications. 
查看全文
Learn how to get started designing a Bluetooth® low energy or Thread IoT product based on NXP's Kinetis KW41Z multi-protocol BLE + 802.15.4 wireless connectivity solution.
查看全文
This class will explain several software solutions offered for the i.MX 8. SafeAssure software allows for a system partitioning that takes full advantage of the ability of some of the safety features of the i.MX 8. Fast Path software allows to route/bridge data between 2 network interfaces in order to maximize data routing performance with minimum CPU load requirements to the main processor. Trusted Environment allows for fully leveraging the Arm® Trustzone capability.
查看全文
Enabling Design, Technologies & Solutions All You Need to Know About DDR4  Boost Your Productivity with CodeWarrior® Development Tools for ARM®v8 Architecture  Hands-On Workshop: General Purpose MCU S32K Deep Dive and S32 SDK  Hands-On Workshop: Kinetis Motor Suite  Hands-On Workshop: MCUXpresso Software and Tools  Hands-On Workshop: MCUXpresso Software and Tools_Lab Guide.pdf  Innovation Made Easy With LPC MCUs: A Roadmap Overview and Deeper Dive Into LPC546xx MCU Family Power Advantages  Introduction to the Next-Generation USB Type-C Connector and NXP’s End-to-End Solution  NFC Integration in Real-Time and Non-Real-Time Operating Systems - Which NFC Product Fits the Best?  NXP’s Next-Generation Layerscape Linux® SDK  NXP’s Sensor Toolbox Ecosystem Overview of the I3C Interface, Successor of the Well-Known I2C Interface  Secure Connected & Automated Vehicles IEC61508 Functional Safety Overview  S32V MPU for Vision, Surround and Fusion Processing  Secure Mobile, Healthcare & Wearables Designing with the New Ultra-Low-Power BLE System on Chip  Smart Buildings & Consumer Goods Google™ Home and NXP®: Android Things, Google Assistant and Chromecast™ Built-in  i.MX 8 Applications Processors Family Overview: i.MX 8, i.MX 8X, i.MX 8M  Low-Power i.MX Applications Processors Overview  Secure Authentication for Anti-Counterfeit Applications  Sensor Products for Medical and Industrial Markets  Voice Control Solutions: Creating Amazon® Alexa® Devices with i.MX  Smart Machinery & Industrial Automation NFC in Industrial and Healthcare—More Use Cases than You Can Imagine  The Next Wave of Industrial Networking with Time Sensitive Networking (TSN)  Smart Networks & Computing Overview of Layerscape 64-bit ARM® Family  San Jose & Westford: Leverage NXP Security and Trust Features for Your System 
查看全文
Low-power wearable/IoT applications are becoming more and more popular. In this session, we will go over some of the key aspects when considering the system-level power management solution for these application, pros and cons when choosing different topologies (for example, DC/DC regulator vs. LDO), overall system level power optimization, and key components selection consideration, etc.
查看全文
The NXP® eIQ™ machine learning software development environment enables the use of ML algorithms on NXP microcontrollers and microprocessors. eIQ software includes inference engines, neural network compilers and optimized libraries. This software not only leverages open-source technologies, it is fully integrated into our MCUXpresso SDK and Yocto development environments, allowing you to develop complete system-level applications with ease.
查看全文
Get to know the latest offering from the leading supplier in Automotive and Industrial controllers. This class will first give you an overview of our benchmark next-generation S32 hardware, software and tool enablement, Then go over the latest product offering of the #1 Automotive MCU S32K with its new reference design, software and tools enablement which will introduce you to the popular and powerful S32V vision processor for mass market applications including new software library enablement for AI CNN and DNN applications.
查看全文
This presentation provides an overview of the new toolchain to support the S32 platform of MCUs and application processors, this includes an IDE with new project generation, extensive collateral for ease of use and getting started as well as the next-generation Debugger tools, a new Flash tool specifically design for the S32 platform, the S32 configuration tool plus numerous software products integrated into the toolchain for ease of customer use.
查看全文
This class will teach you how to spin a BLDC, PMSM or ACIM motor with i.MX RT. You do not need prior motor control experience.
查看全文
Design, Software & Services APF-DES-T2229 - Kinetis New Products, KE+, Security with K8x & KL8x  Secure Connected & Automated Vehicles APF-AUT-T2295 - Hands-On Workshop: How to Tune a New PMSM Step-by-Step  Secure Mobile, Healthcare & Wearables APF-MHW-T2232 - LPC541xx for Wearable
查看全文
Time-sensitive automotive Ethernet network can increase the precision, reliability, robustness and network security of in-vehicle network and enhance the way toward autonomous driving. The NXP SJA1105x family is one of first TSN-capable automotive Ethernet switches. It can support: IEEE® 802.1Qbv time-aware shaping and the IEEE 802.1Qci per-stream policing. During the presentation, the use cases of core TSN specifications will be discussed.
查看全文
EUF-NET-T1745 - An overview of ARMv8 virtualization technology, its integration in NXP Layerscape ARMv8-based SoC's and its enablement through the QorIQ SDK .
查看全文
Hands-on starting with the i.MX 8M Mini EVK, we will cover the out-of-the-box enablement including software, tools, hardware design guides, and demonstration software. Attendees should leave this class with the confidence to start their own design using the i.MX 8M Mini.
查看全文
NXP increasingly offers a broad variety of software components, product, professional support and services. This section will describe, based on customer use case how NXP can help accelerate time to market and de-risk project development thanks to our professional support and services teams.
查看全文
Getting started with MCUXpresso SDK, IDE, and Config tools.
查看全文
Extending the scalable range of the i.MX product line, the i.MX 8 series establishes an unmatched range of cost-performance scaling with pin-compatible options and the highest level of software reuse. Built with a high-level integration to support graphics, video, image processing, vision, audio and voice functions, the i.MX 8 series transforms your everyday interactions. Preview the next generation i.MX 8 series applications processors for Automotive, Consumer and Industrial applications.
查看全文
In automotive applications, it is typical to have a central processing unit that interfaces with other peripheral devices, other sub-systems and the user. Often, the signals from these interconnects may be incompatible on both ends. Therefore, various semiconductor devices such as analog switches, voltage level translators, and GPIO expanders are often used to bridge between the interconnects on the board. Also, LED Controllers, LCD Drivers and Real Time Clocks are used for interfacing between the system and user. In this session, we will explore the application of these analog and interface devices from NXP and discuss their applications in automotive applications.
查看全文