License for CodeWarrior TAP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

License for CodeWarrior TAP

2,737件の閲覧回数
alcodextech
Contributor I

how and where do i buy license for CodeWarrior TAP for debugging and flashing purposes only?

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,365件の閲覧回数
TomasPaez
NXP Employee
NXP Employee

Alcodex,

Let us know which device are you using the CW TAP so we can point you to the right version to use and their license models.

Thank you

0 件の賞賛
返信

2,365件の閲覧回数
alcodextech
Contributor I

MPC8308

0 件の賞賛
返信

2,365件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

For MPC8308, the supported CodeWarrior tool is:

CodeWarrior Development Tools for PowerQUICC|Freescale

You need Developer Suite Level or higher to debugger MPC8308, for details, please refer to:

http://cache.freescale.com/files/soft_dev_tools/doc/fact_sheet/CWDEVSNETAPPFS.pdf

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,365件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Alcodex,

In order to use the CodeWarrior TAP for debugging and flashing you first you need to acquire a CodeWarrior Development suite. On the following link you will find the CodeWarrior Development Suites information:

CodeWarrior Suites (Bas, Stand, Pro)|Freescale

Here is a video that explains how to register your new software suite and where to find the license and product installers:

How to register & activate my software|Freescale

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------