MMA8452QR1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MMA8452QR1

跳至解决方案
2,680 次查看
abialevich1
Contributor II

Good morning Team,

MMA8452QR1 is this obsolete component? If yes, any alternative options like-for-like available?

标记 (1)
1 解答
2,650 次查看
diazmarin09
NXP TechSupport
NXP TechSupport

Hello abialevich1,

I hope all is great with you. Thank you for using the NXP communities.

You are correct, the MMA8452Q device is obsolete. Unfortunately, we do not have a direct replacement. I mean, pin-to-pin compatible.

In this case, I would like to recommend the following series from our accelerometer portfolio:

FXLS8967AF - ±2g/±4g/±8g/±16g, Low Power 12-bit Digital Accelerometer

I hope this information helps.

Regards,

David

在原帖中查看解决方案

5 回复数
2,651 次查看
diazmarin09
NXP TechSupport
NXP TechSupport

Hello abialevich1,

I hope all is great with you. Thank you for using the NXP communities.

You are correct, the MMA8452Q device is obsolete. Unfortunately, we do not have a direct replacement. I mean, pin-to-pin compatible.

In this case, I would like to recommend the following series from our accelerometer portfolio:

FXLS8967AF - ±2g/±4g/±8g/±16g, Low Power 12-bit Digital Accelerometer

I hope this information helps.

Regards,

David

2,358 次查看
jridings1
Contributor IV

Rochester Electronics has partnered with NXP Motion Sensor team to offer EOL products. We have acquired extensive authorized NXP inventory on MMA8452QR1/MMA8453Q1/MMA8451Q1. Please visit www.rocelec.com to view our extensive NXP Accelerometer inventory. 

0 项奖励
回复
2,496 次查看
abialevich1
Contributor II

Do you have something available that meets or exceeds the "sensitivity change versus temperature" and "zero-g level change versus temperature" of the MMA8452QR1?

标记 (1)
2,345 次查看
onyourlight
Contributor III

MMA8452QR1 has sufficient stock, it is not recommended that you replace it, 1$

0 项奖励
回复
2,338 次查看
jridings1
Contributor IV

2.4Mu at www.rocelec.com

 

0 项奖励
回复