MMA8452QR1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,654件の閲覧回数
abialevich1
Contributor II

Good morning Team,

MMA8452QR1 is this obsolete component? If yes, any alternative options like-for-like available?

タグ(1)
1 解決策
2,624件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello abialevich1,

I hope all is great with you. Thank you for using the NXP communities.

You are correct, the MMA8452Q device is obsolete. Unfortunately, we do not have a direct replacement. I mean, pin-to-pin compatible.

In this case, I would like to recommend the following series from our accelerometer portfolio:

FXLS8967AF - ±2g/±4g/±8g/±16g, Low Power 12-bit Digital Accelerometer

I hope this information helps.

Regards,

David

元の投稿で解決策を見る

5 返答(返信)
2,625件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello abialevich1,

I hope all is great with you. Thank you for using the NXP communities.

You are correct, the MMA8452Q device is obsolete. Unfortunately, we do not have a direct replacement. I mean, pin-to-pin compatible.

In this case, I would like to recommend the following series from our accelerometer portfolio:

FXLS8967AF - ±2g/±4g/±8g/±16g, Low Power 12-bit Digital Accelerometer

I hope this information helps.

Regards,

David

2,332件の閲覧回数
jridings1
Contributor IV

Rochester Electronics has partnered with NXP Motion Sensor team to offer EOL products. We have acquired extensive authorized NXP inventory on MMA8452QR1/MMA8453Q1/MMA8451Q1. Please visit www.rocelec.com to view our extensive NXP Accelerometer inventory. 

0 件の賞賛
返信
2,470件の閲覧回数
abialevich1
Contributor II

Do you have something available that meets or exceeds the "sensitivity change versus temperature" and "zero-g level change versus temperature" of the MMA8452QR1?

タグ(1)
2,319件の閲覧回数
onyourlight
Contributor III

MMA8452QR1 has sufficient stock, it is not recommended that you replace it, 1$

0 件の賞賛
返信
2,312件の閲覧回数
jridings1
Contributor IV

2.4Mu at www.rocelec.com

 

0 件の賞賛
返信