VR5510-FMEDA-external circuit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VR5510-FMEDA-external circuit

ソリューションへジャンプ
795件の閲覧回数
zeyu_yan
Contributor III

Hello, when I analyse the external circuit of VR5510 and calculate the FMEDA of the system,how can I integrate the FMEDA of VR5510 into my system FMEDA?

for example the function block:High voltage buck,Vpre, the MOS Q1 and Q2 has the failure mode and fit

PRE-Regulator has the failure mode and fit.

Accourding to failure mode (regulaterd output  in OV UV drift ...)descripted in sheet<FMEDA_PM>,it seems the sub block <PRE-REGULATOR> includes the external MOSFET of Q1 and Q2.image.pngimage.png

 

 

 

タグ(2)
0 件の賞賛
1 解決策
788件の閲覧回数
r40959
NXP Employee
NXP Employee
Hello the HV buck in the FMEDA (VR5510) is not including the external FET. We stop our quantitative analyis to to pinout and we don't consider the ext components. The suggestion is that you use the FMEDA VR5510 in addition to your bill of materials (Q1, Q2 and i guess others you might have). In case you have a doubt of the effect and safety mechanism that will be efficient, please let us know, we can support. Hoping it helps, thank you best regards Valerie

元の投稿で解決策を見る

0 件の賞賛
1 返信
789件の閲覧回数
r40959
NXP Employee
NXP Employee
Hello the HV buck in the FMEDA (VR5510) is not including the external FET. We stop our quantitative analyis to to pinout and we don't consider the ext components. The suggestion is that you use the FMEDA VR5510 in addition to your bill of materials (Q1, Q2 and i guess others you might have). In case you have a doubt of the effect and safety mechanism that will be efficient, please let us know, we can support. Hoping it helps, thank you best regards Valerie
0 件の賞賛