VR5510-FMEDA-external circuit

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

VR5510-FMEDA-external circuit

跳至解决方案
790 次查看
zeyu_yan
Contributor III

Hello, when I analyse the external circuit of VR5510 and calculate the FMEDA of the system,how can I integrate the FMEDA of VR5510 into my system FMEDA?

for example the function block:High voltage buck,Vpre, the MOS Q1 and Q2 has the failure mode and fit

PRE-Regulator has the failure mode and fit.

Accourding to failure mode (regulaterd output  in OV UV drift ...)descripted in sheet<FMEDA_PM>,it seems the sub block <PRE-REGULATOR> includes the external MOSFET of Q1 and Q2.image.pngimage.png

 

 

 

标记 (2)
0 项奖励
1 解答
783 次查看
r40959
NXP Employee
NXP Employee
Hello the HV buck in the FMEDA (VR5510) is not including the external FET. We stop our quantitative analyis to to pinout and we don't consider the ext components. The suggestion is that you use the FMEDA VR5510 in addition to your bill of materials (Q1, Q2 and i guess others you might have). In case you have a doubt of the effect and safety mechanism that will be efficient, please let us know, we can support. Hoping it helps, thank you best regards Valerie

在原帖中查看解决方案

0 项奖励
1 回复
784 次查看
r40959
NXP Employee
NXP Employee
Hello the HV buck in the FMEDA (VR5510) is not including the external FET. We stop our quantitative analyis to to pinout and we don't consider the ext components. The suggestion is that you use the FMEDA VR5510 in addition to your bill of materials (Q1, Q2 and i guess others you might have). In case you have a doubt of the effect and safety mechanism that will be efficient, please let us know, we can support. Hoping it helps, thank you best regards Valerie
0 项奖励