S32K344 FMEDA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K344 FMEDA

Jump to solution
3,133 Views
shuaishuaifei
Contributor II

Hi NXP

1.where can I get FMEDA files of S32K344、MC33664ATL1RG、TJA1042T/3、MC33879APEK、MC33775AT.

2.I have got the FMEDA SEooC Static - S32K344  file, but how can we calculate our FIT value according our bms application. thanks.

 

0 Kudos
1 Solution
3,113 Views
shuaishuaifei
Contributor II

hi r40959 naveenm

where can we find FIT value of MC33664, MC33879, TJA1042? thanks.

View solution in original post

0 Kudos
8 Replies
3,114 Views
shuaishuaifei
Contributor II

hi r40959 naveenm

where can we find FIT value of MC33664, MC33879, TJA1042? thanks.

0 Kudos
3,103 Views
r40959
NXP Employee
NXP Employee

Hello,

unfortunately the FIT rate were not evaluated on those devices. Do you have a way to evaluate on your side if we provide to you the range of transistor count of those devices ?

let us know,

best regards,

 

0 Kudos
3,100 Views
shuaishuaifei
Contributor II

Hello,

ok,please provide the transistor count range for these devices.thanks

0 Kudos
3,086 Views
r40959
NXP Employee
NXP Employee

Hello,

 

MC33664 transitor count is in the range 50k-500k referring to table 5 of SN29500

TJA1042 in the category >3k referring to table 4 of SN29500

MC33879 in the category 50k-500k referring to table 5 of SN29500

thank you

best regards

0 Kudos
3,079 Views
shuaishuaifei
Contributor II

hello,

thank you very much

0 Kudos
3,119 Views
shuaishuaifei
Contributor II

hi r40959 naveenm

thank you very much.

we have another question. Could you help us?

where can we find FIT value of MC33664, MC33879, TJA1042? thanks.

0 Kudos
3,127 Views
r40959
NXP Employee
NXP Employee

Hello,

 

you can find for MC33775A in NXP DocStore website the Safety analysis report with FMEDA HW architectural metrics results "Rp698910 - Safety Analysis Report MC33775A (1.0)"

However, the MC33664, MC33879, TJA1042 are QM (Quality Managed) Auto AECQ100 products for which we don't produce a FMEDA as they are not developed according to ISO26262.

Hoping it helps you,

thank you

Best regards,

Valerie Bernon

 

0 Kudos
3,125 Views
naveenm
NXP Employee
NXP Employee

Answer to Q2: 

I have got the FMEDA SEooC Static - S32K344  file, but how can we calculate our FIT value according our bms application. thanks.

 

A2: The FIT is calculated as illustrated in ISO 26262 documentation, chapter 11 (ISO 26262-11:2018(E)) Section "4.6.2 Permanent base failure rate calculation methods"

 

Hope it helps.

Regards,

NaveenM

Tags (1)
0 Kudos