S32K344 FMEDA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,158件の閲覧回数
shuaishuaifei
Contributor II

Hi NXP

1.where can I get FMEDA files of S32K344、MC33664ATL1RG、TJA1042T/3、MC33879APEK、MC33775AT.

2.I have got the FMEDA SEooC Static - S32K344  file, but how can we calculate our FIT value according our bms application. thanks.

 

0 件の賞賛
1 解決策
3,138件の閲覧回数
shuaishuaifei
Contributor II

hi r40959 naveenm

where can we find FIT value of MC33664, MC33879, TJA1042? thanks.

元の投稿で解決策を見る

0 件の賞賛
8 返答(返信)
3,139件の閲覧回数
shuaishuaifei
Contributor II

hi r40959 naveenm

where can we find FIT value of MC33664, MC33879, TJA1042? thanks.

0 件の賞賛
3,128件の閲覧回数
r40959
NXP Employee
NXP Employee

Hello,

unfortunately the FIT rate were not evaluated on those devices. Do you have a way to evaluate on your side if we provide to you the range of transistor count of those devices ?

let us know,

best regards,

 

0 件の賞賛
3,125件の閲覧回数
shuaishuaifei
Contributor II

Hello,

ok,please provide the transistor count range for these devices.thanks

0 件の賞賛
3,111件の閲覧回数
r40959
NXP Employee
NXP Employee

Hello,

 

MC33664 transitor count is in the range 50k-500k referring to table 5 of SN29500

TJA1042 in the category >3k referring to table 4 of SN29500

MC33879 in the category 50k-500k referring to table 5 of SN29500

thank you

best regards

0 件の賞賛
3,104件の閲覧回数
shuaishuaifei
Contributor II

hello,

thank you very much

0 件の賞賛
3,144件の閲覧回数
shuaishuaifei
Contributor II

hi r40959 naveenm

thank you very much.

we have another question. Could you help us?

where can we find FIT value of MC33664, MC33879, TJA1042? thanks.

0 件の賞賛
3,152件の閲覧回数
r40959
NXP Employee
NXP Employee

Hello,

 

you can find for MC33775A in NXP DocStore website the Safety analysis report with FMEDA HW architectural metrics results "Rp698910 - Safety Analysis Report MC33775A (1.0)"

However, the MC33664, MC33879, TJA1042 are QM (Quality Managed) Auto AECQ100 products for which we don't produce a FMEDA as they are not developed according to ISO26262.

Hoping it helps you,

thank you

Best regards,

Valerie Bernon

 

0 件の賞賛
3,150件の閲覧回数
naveenm
NXP Employee
NXP Employee

Answer to Q2: 

I have got the FMEDA SEooC Static - S32K344  file, but how can we calculate our FIT value according our bms application. thanks.

 

A2: The FIT is calculated as illustrated in ISO 26262 documentation, chapter 11 (ISO 26262-11:2018(E)) Section "4.6.2 Permanent base failure rate calculation methods"

 

Hope it helps.

Regards,

NaveenM

タグ(1)
0 件の賞賛