i2c do not send the message in the project example "lpi2c_master_s32k144"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i2c do not send the message in the project example "lpi2c_master_s32k144"

ソリューションへジャンプ
925件の閲覧回数
adrimen3668
Contributor II

Hello,

We are trying to use the project example "lpi2c_master_s32k144" and we can not see the i2c signal with the oscilloscope in this line.

adrimen3668_0-1677752543474.png

We are using an external pull-up for the scl and sda connected to 3.3 volts. 

We tried also with 5 volts.

adrimen3668_2-1677752741239.png

Thanks in advance.

 

 

0 件の賞賛
返信
1 解決策
915件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @adrimen3668,

The J2.19, J2.20 are not routed to PTA2/PTA3 by default.

Use J1.1, J1.3 instead.

danielmartynek_1-1677756883801.png

 

 

BR, Daniel

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
916件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @adrimen3668,

The J2.19, J2.20 are not routed to PTA2/PTA3 by default.

Use J1.1, J1.3 instead.

danielmartynek_1-1677756883801.png

 

 

BR, Daniel

 

0 件の賞賛
返信