i2c do not send the message in the project example "lpi2c_master_s32k144"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i2c do not send the message in the project example "lpi2c_master_s32k144"

Jump to solution
950 Views
adrimen3668
Contributor II

Hello,

We are trying to use the project example "lpi2c_master_s32k144" and we can not see the i2c signal with the oscilloscope in this line.

adrimen3668_0-1677752543474.png

We are using an external pull-up for the scl and sda connected to 3.3 volts. 

We tried also with 5 volts.

adrimen3668_2-1677752741239.png

Thanks in advance.

 

 

0 Kudos
Reply
1 Solution
940 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @adrimen3668,

The J2.19, J2.20 are not routed to PTA2/PTA3 by default.

Use J1.1, J1.3 instead.

danielmartynek_1-1677756883801.png

 

 

BR, Daniel

 

View solution in original post

0 Kudos
Reply
1 Reply
941 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @adrimen3668,

The J2.19, J2.20 are not routed to PTA2/PTA3 by default.

Use J1.1, J1.3 instead.

danielmartynek_1-1677756883801.png

 

 

BR, Daniel

 

0 Kudos
Reply