Siul2_Port_Ip_Init & Hi-Z

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Siul2_Port_Ip_Init & Hi-Z

跳至解决方案
2,458 次查看
jetty_1012
Contributor II

Hi,

I have configured some ports on S32 DS.

And I know this API Siul2_Port_Ip_Init is used to initialize the ports.

My questioin is, if the ports that I configured on S32 DS are not initialized, are they Hi-Z?

 

Thanks,

Jetty

0 项奖励
回复
1 解答
2,436 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @jetty_1012 

When you don't configure a pin, it maintains the same state it has after a power-up. 

Please refer to section 4.5 (Pin States) of the S32K3xx Reference Manual, Rev. 6.

 

B.R.

VaneB

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,437 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @jetty_1012 

When you don't configure a pin, it maintains the same state it has after a power-up. 

Please refer to section 4.5 (Pin States) of the S32K3xx Reference Manual, Rev. 6.

 

B.R.

VaneB

0 项奖励
回复