Siul2_Port_Ip_Init & Hi-Z

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Siul2_Port_Ip_Init & Hi-Z

Jump to solution
510 Views
jetty_1012
Contributor II

Hi,

I have configured some ports on S32 DS.

And I know this API Siul2_Port_Ip_Init is used to initialize the ports.

My questioin is, if the ports that I configured on S32 DS are not initialized, are they Hi-Z?

 

Thanks,

Jetty

0 Kudos
1 Solution
488 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @jetty_1012 

When you don't configure a pin, it maintains the same state it has after a power-up. 

Please refer to section 4.5 (Pin States) of the S32K3xx Reference Manual, Rev. 6.

 

B.R.

VaneB

View solution in original post

0 Kudos
1 Reply
489 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @jetty_1012 

When you don't configure a pin, it maintains the same state it has after a power-up. 

Please refer to section 4.5 (Pin States) of the S32K3xx Reference Manual, Rev. 6.

 

B.R.

VaneB

0 Kudos