Hi,
I have configured some ports on S32 DS.
And I know this API Siul2_Port_Ip_Init is used to initialize the ports.
My questioin is, if the ports that I configured on S32 DS are not initialized, are they Hi-Z?
Thanks,
Jetty
解決済! 解決策の投稿を見る。
Hi @jetty_1012
When you don't configure a pin, it maintains the same state it has after a power-up.
Please refer to section 4.5 (Pin States) of the S32K3xx Reference Manual, Rev. 6.
B.R.
VaneB
元の投稿で解決策を見る