Hi
Sorry for the late reply.
DMA sources called slots can be found in DMA_CH_MUX of S32K1xx_DMA_Interrupt_mapping.xlsx.
Do you want to use BAUD[TDMAE] configures the transmit data register empty flag, STAT[TDRE], to generate a DMA request? (Peripheral request)Slot_Num 3 is the Transmit DMA Request of LPUART0.

TRGMUX_IN0 belong to Trigger not Peripheral request. Seems that you want to achieve 17.4.1 DMA channels with periodic triggering capability.

I'm not sure what specific functionality you want to achieve. May I ask if it is the S32K LPUART hardware flow control?
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------