S32 DS USing ADC without interrupt on the S32K311

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32 DS USing ADC without interrupt on the S32K311

1,305 次查看
SAL_111
Contributor II

Hi, I'm using the S32K311 microcontroller, I successfully read in 18 analog inputs (6 channels o ADC0 and 12 channels on ADC1), the ADCs are triggered by the PIT to perform continous measurements, now I want to implement a solution without interrupts, I want to use DMA, but I found one example here in the community, but maybe there is someone out ther because the sample reads 5 ADC channels from one ADC only, how can I read 18 channels, how do I have to configure the DMA driver for this, I want to use BCTU, PIT and DMA to perform the ADC conversions.

0 项奖励
回复
4 回复数

1,244 次查看
SAL_111
Contributor II

How can I use the DMA driver without any interrupt, so that in my application I only would have the interrupt of the PIT and not from the ADC or DMA or anything else so far

Furthermore, how is it possible to read 6 channels on ADC0 and 12 channels on ADC1 with the BCTU, because it can read parallel, but then I would also have to read 12 channels on ADC0 so the result array has the correct values for both ADCs

0 项奖励
回复

1,163 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if remember well, a if BCTU FIFO is used a driver needs to have DMA interrupt enabled, so DMA request is reenabled. Unless you will modify RTD code.

If you need to trigger different number of channels on ADC modules then you will need to use separate BCTU triggers for that and those will point to different channel lists.
Maybe it could be better to do parallel conversions and sample again same channels on ADC0 redundantly.

BR, Petr

0 项奖励
回复

1,300 次查看
SAL_111
Contributor II

Adding info current status through the PIT interrupt i read ADC0 with interrupt and ADC1 with interrupt, now I only want to have the interrupt of the PIT, so I need to get the 18 ADC measurements from the DMA

0 项奖励
回复