Interrupt based message configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Interrupt based message configuration

2,768件の閲覧回数
AparnaSridharan
Contributor II

Hi,

Actually I need to create interrupt for function when a receive particular message id. Is there anyway i can do this for S32k144 board with S32ds.

0 件の賞賛
返信
4 返答(返信)

2,762件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@AparnaSridharan

The easiest way is to judge the data you need among all the received data

you can take a look at the revevant registers in the picture below.

Senlent_0-1649772158721.pngSenlent_0-1649772158721.png

I don't know if this register can achieve the function you want,and there is no demo program for your reference,

BR!

      Jim,

0 件の賞賛
返信

2,752件の閲覧回数
AparnaSridharan
Contributor II

Hi @Senlent ,

AparnaSridharan_0-1649826816016.pngAparnaSridharan_0-1649826816016.png

 

Actually I need to invoke an interrupt for a function when I receive particular CAN id which will stay continuously in receive function till all the lines in the configuration_function() get completed. For this whether I can use LPUART match register. 

0 件の賞賛
返信

2,748件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@AparnaSridharan 

       I'm a little confused, your first question is related to uart, I can't understand what your second question has to do with uart? Your second question is simple, FlexCAN can support certain frame transceiving interrupts.

BR!

      Jim,

0 件の賞賛
返信

2,746件の閲覧回数
AparnaSridharan
Contributor II

Hi @Senlent ,

Actually What i need is I need to create a interrupt for a flex_CAN receive function. That interrupt need to be enabled only when particular CAN message id is received. After enabling the interrupt the control need to be there inside the receive function till interrupt is disabled.

タグ(1)
0 件の賞賛
返信