FlexNVM Memory data retention ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FlexNVM Memory data retention ?

ソリューションへジャンプ
2,951件の閲覧回数
Ahmad_bozorgi
Contributor II

Hi.

with refer to S32K1xx datasheet, in 6.3.1.2 Reliability specifications  data retention of FlexNVM memories mentioned:

Capture.JPGCapture.JPG

 

respect to S32K144 FlexRAM & FlexNVM capacity which is 4KB & 64KB, so EEPROM backup to FlexRAM ratio in best situation will be 16. write endurance for these setting is at least 100K. data retention is 5 years.

1. Data retention after up to 1 K cycles is 20 years min. if we use half of D_Flash as FlexRAM backup and other for normal write (doing by software), how will be D-Flash data retention time ? (assuming linear relationship e.g. write/erase cycling of 100K)

2. if we write some locations of D-Flash for e.g. 50K and other locations for 1K, data retention time for these two locations is different ? (assume they are not in same block).

3. if we write/erase FlexRAM for e.g. 60K and after that these operations stops, data retention is same as previous?

Thanks.

0 件の賞賛
返信
1 解決策
2,939件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Ahmad,

You are referring to an old datasheet, please use the latest rev.13

danielmartynek_0-1601559231855.pngdanielmartynek_0-1601559231855.png

The ratio can be > 16 if you don't use the whole FlexRAM (less than 4kB of records in FlexRAM).

Please use the Flex Memory Endurance Calculator.

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/s32k-automotive-mc...

danielmartynek_1-1601559551228.pngdanielmartynek_1-1601559551228.png

 

The EEPROM retention is specified as 20 years for 10% of the calculated endurance.

 

1 & 2.

The DFlash endurance is 1k max, Table 38, footnote 6.

3.

As specified, 5 or 20 years, depending on the calculated endurance.

 

Best regards,

Daniel

 

 

 

.

 

元の投稿で解決策を見る

1 返信
2,940件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Ahmad,

You are referring to an old datasheet, please use the latest rev.13

danielmartynek_0-1601559231855.pngdanielmartynek_0-1601559231855.png

The ratio can be > 16 if you don't use the whole FlexRAM (less than 4kB of records in FlexRAM).

Please use the Flex Memory Endurance Calculator.

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/s32k-automotive-mc...

danielmartynek_1-1601559551228.pngdanielmartynek_1-1601559551228.png

 

The EEPROM retention is specified as 20 years for 10% of the calculated endurance.

 

1 & 2.

The DFlash endurance is 1k max, Table 38, footnote 6.

3.

As specified, 5 or 20 years, depending on the calculated endurance.

 

Best regards,

Daniel

 

 

 

.