FlexNVM Memory data retention ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FlexNVM Memory data retention ?

Jump to solution
3,015 Views
Ahmad_bozorgi
Contributor II

Hi.

with refer to S32K1xx datasheet, in 6.3.1.2 Reliability specifications  data retention of FlexNVM memories mentioned:

Capture.JPG

 

respect to S32K144 FlexRAM & FlexNVM capacity which is 4KB & 64KB, so EEPROM backup to FlexRAM ratio in best situation will be 16. write endurance for these setting is at least 100K. data retention is 5 years.

1. Data retention after up to 1 K cycles is 20 years min. if we use half of D_Flash as FlexRAM backup and other for normal write (doing by software), how will be D-Flash data retention time ? (assuming linear relationship e.g. write/erase cycling of 100K)

2. if we write some locations of D-Flash for e.g. 50K and other locations for 1K, data retention time for these two locations is different ? (assume they are not in same block).

3. if we write/erase FlexRAM for e.g. 60K and after that these operations stops, data retention is same as previous?

Thanks.

0 Kudos
Reply
1 Solution
3,003 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Ahmad,

You are referring to an old datasheet, please use the latest rev.13

danielmartynek_0-1601559231855.png

The ratio can be > 16 if you don't use the whole FlexRAM (less than 4kB of records in FlexRAM).

Please use the Flex Memory Endurance Calculator.

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/s32k-automotive-mc...

danielmartynek_1-1601559551228.png

 

The EEPROM retention is specified as 20 years for 10% of the calculated endurance.

 

1 & 2.

The DFlash endurance is 1k max, Table 38, footnote 6.

3.

As specified, 5 or 20 years, depending on the calculated endurance.

 

Best regards,

Daniel

 

 

 

.

 

View solution in original post

1 Reply
3,004 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Ahmad,

You are referring to an old datasheet, please use the latest rev.13

danielmartynek_0-1601559231855.png

The ratio can be > 16 if you don't use the whole FlexRAM (less than 4kB of records in FlexRAM).

Please use the Flex Memory Endurance Calculator.

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/s32k-automotive-mc...

danielmartynek_1-1601559551228.png

 

The EEPROM retention is specified as 20 years for 10% of the calculated endurance.

 

1 & 2.

The DFlash endurance is 1k max, Table 38, footnote 6.

3.

As specified, 5 or 20 years, depending on the calculated endurance.

 

Best regards,

Daniel

 

 

 

.