FS26 SBC debug hardware connections

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS26 SBC debug hardware connections

1,393 Views
mogilipuri_harish
Contributor II

hello team

 

we are using FS26 SBC. we need help for hardware connection for debug pin in FS26 SBC.

0 Kudos
Reply
3 Replies

1,376 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello,

I hope all is great with you. Thank you for using the NXP communities.

To enter in OTP Mode, the voltage on pin DEBUG must be set at VOTP (7.4V < debug pin < 8.4V) prior to apply any voltage on VSUP pin.

The debug mode can be used during customer production process. This mode can be access by applying VDBG (2.5V <Debug pin < 6V) on debug pin prior to apply any voltage to VSUP.

Therefore, I do recommend applying a circuit based on the requirements of your design. I mean, if you need both OTP and debug mode, you may place a jumper for selecting the voltage source for example. You may also include a RC filter at the DEBUG pin.

If you have an NDA number, please let me know. I can share with you further information (confidential).

I hope this information helps.

Regards,

David

0 Kudos
Reply

1,367 Views
mogilipuri_harish
Contributor II

hello

this is my NDA no: 7e8f5683-eff2-42b8-8f60-0ecda241eea4

0 Kudos
Reply

1,359 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello,

Unfortunately, I am not able to validate your NDA number.

Could you please submit a new case in order to review your NDA?

Thank you for your understanding.

Regards,

David

0 Kudos
Reply