FS26 FAQ: SPI Protocol Configuration is not sync with current FS26 implementation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

FS26 FAQ: SPI Protocol Configuration is not sync with current FS26 implementation

跳至解决方案
2,023 次查看
cuongnguyenphu
NXP Employee
NXP Employee

Document si849710-FS26 FAQ Frequently Asked Questions(1.0).pdf mentioned about SPI configuration as following:

cuongnguyenphu_0-1716781666606.png

However, in current implemented code it will get fail if setup SPI configuration like that:
[C:\EB\tresos29\..\..\NXP\S32K3_FS26_R21-11_2.0.0_CD01\eclipse\plugins\Sbc_fs26_TS_T40D34M20I0R0/generate_PB/src/CDD_Sbc_fs26_PBcfg.c (signed):25]:
"The selected SpiChannelRef must has SpiDataWidth equal to 8"

It needs to update the document FS26 FAQ again to sync-up with current implementation code

cuongnguyenphu_1-1716781698779.png

 

0 项奖励
回复
1 解答
1,957 次查看
cuongnguyenphu
NXP Employee
NXP Employee

Discussed internally  
FAQ will be updated later

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,958 次查看
cuongnguyenphu
NXP Employee
NXP Employee

Discussed internally  
FAQ will be updated later

0 项奖励
回复
1,993 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Discussed internally with the author of the FS26 FAQ document.

The fact is that the FS26 uses a 32-bit SPI, with the following arrangement:

MOSI (Main Out, Secondary In) bits:
• Bit 31: Main or fail-safe registers selection
• Bit 30 to 25: Register address• Bit 24: Read/Write (For reading Bit 24 = 0; For writing Bit 24 = 1)
• Bit 23 to 8: Control bits
• Bit 7 to 0: Cyclic redundant check (CRC)

MISO (Main In, Secondary Out) bits:
• Bit 31-24: General device status
• Bits 23 to 8: Extended device status, or device internal control register content or device flags 
• Bit 7 to 0: Cyclic redundant check (CRC)

BRs, Tomas

0 项奖励
回复