Cannot Rename my project [S32DS v3.4]

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cannot Rename my project [S32DS v3.4]

ソリューションへジャンプ
2,988件の閲覧回数
gpira
Contributor III

 

Hi everyone,

I want to rename my project from 'UNC_0_0_0a0' to 'UNC_1_0_0a0', but it gives me this error.

'BSW0_0_0a0' was the name of the original project from which I started to develop the current one.

The project is already in the workspace, since I've read that otherwise the renaming won't be possible,

but it doesn't work anyway.

I don't know what to do, anyone can help me?

Thanks in advance.

Best regards, 

Giacomo

gpira_0-1650380999084.pnggpira_0-1650380999084.png

 

 

 

0 件の賞賛
返信
1 解決策
2,972件の閲覧回数
gpira
Contributor III

Nevermind, I found  a solution.

I had to modify the project name in the ".project" file, contained in the project folder.

Once I aligned it with my folder name (from BSW0_0_0a0 to UNC_0_0_0a0) I was able to

rename it again, using the Rename command.

Hope this will be helpful for someone.

Best Regards,

Giacomo

元の投稿で解決策を見る

2 返答(返信)
2,461件の閲覧回数
Nitrogen8212
Contributor I

Thank you!

0 件の賞賛
返信
2,973件の閲覧回数
gpira
Contributor III

Nevermind, I found  a solution.

I had to modify the project name in the ".project" file, contained in the project folder.

Once I aligned it with my folder name (from BSW0_0_0a0 to UNC_0_0_0a0) I was able to

rename it again, using the Rename command.

Hope this will be helpful for someone.

Best Regards,

Giacomo