Cannot Rename my project [S32DS v3.4]

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Cannot Rename my project [S32DS v3.4]

跳至解决方案
3,015 次查看
gpira
Contributor III

 

Hi everyone,

I want to rename my project from 'UNC_0_0_0a0' to 'UNC_1_0_0a0', but it gives me this error.

'BSW0_0_0a0' was the name of the original project from which I started to develop the current one.

The project is already in the workspace, since I've read that otherwise the renaming won't be possible,

but it doesn't work anyway.

I don't know what to do, anyone can help me?

Thanks in advance.

Best regards, 

Giacomo

gpira_0-1650380999084.png

 

 

 

0 项奖励
回复
1 解答
2,999 次查看
gpira
Contributor III

Nevermind, I found  a solution.

I had to modify the project name in the ".project" file, contained in the project folder.

Once I aligned it with my folder name (from BSW0_0_0a0 to UNC_0_0_0a0) I was able to

rename it again, using the Rename command.

Hope this will be helpful for someone.

Best Regards,

Giacomo

在原帖中查看解决方案

2 回复数
2,488 次查看
Nitrogen8212
Contributor I

Thank you!

0 项奖励
回复
3,000 次查看
gpira
Contributor III

Nevermind, I found  a solution.

I had to modify the project name in the ".project" file, contained in the project folder.

Once I aligned it with my folder name (from BSW0_0_0a0 to UNC_0_0_0a0) I was able to

rename it again, using the Rename command.

Hope this will be helpful for someone.

Best Regards,

Giacomo