S32K Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K Knowledge Base

Labels

Discussions

Sort by:
Hi,     If you try to compile the sample project within S32K14X_MCAL4_2_RTM_1_0_0, you should take care of the command if you use Linaro.    After you set the environment of compiling and run the command under command window, you should enter     "launch.bat MODE=USER TOOLCHAIN=linaro"    NOT    "launch.bat MODE=USER TOOLCHAIN=LINARO"      The command is case sensitivity.   Hope you can compile the project successfully.  Cheers! Oliver
View full article
Hi,        ARM Cortex-M have a DWT (Data Watchpoint and Trace) unit implemented, and it has a nice feature in that unit which counts the execution cycles. The DWT is usually implemented on most Cortex-M3, M4 and M7 devices, including e.g. the NXP S32K14x.      Attachment is the sample project on S32K142 to measure the running time of a function.     Password of extraction is nxp.     Enjoy the measuring!   Cheers! Oliver BTW, Measure the running time of one function on PowerPC could also be gotten through the link.
View full article
******************************************************************************** * Detailed Description: * This simple example shows how to force function to RAM memory in S32 Design * Studio and how to perform flash functions (Erase flash sector and Program * phrase command in this case). * * ------------------------------------------------------------------------------ * Test HW:         FRDM-S32K144 * MCU:             PS32K144HFVLL 0N77P * Fsys:            default * Debugger:        Lauterbach Trace32 * Target:          internal_FLASH * ********************************************************************************
View full article
******************************************************************************** * Detailed Description: * RAM self-test is performed after reset in startup_S32K144.s file. * The RAM self-test should be executed right after reset, so it does not destroy * data loaded to RAM by init functions. The code is inserted after * initialization of core registers. RAM initialization is commented out because * the same operation is done by the self-test. * The test flow is: * 1. Write pattern 0x55AA55AA to first word in RAM * 2. Read the data back * 3. Compare the data and increment error counter if not equal * 4. Write inverse pattern 0xAA55AA55 to first word in RAM * 5. Read the data back * 6. Compare the data and increment error counter if not equal * 7. Clear the first word in RAM to leave whole RAM erased to ‘0’ at the end of test * This procedure is repeated for whole RAM. * If the error counter is different from zero at the end, the program stays in * endless loop until watchdog reset. * * ------------------------------------------------------------------------------ * Test HW:         S32K144EVB-Q100 * MCU:             FS32K144UAVLL 0N57U * Fsys:            Default * Debugger:        Lauterbach Trace32 * Target:          internal_FLASH * ********************************************************************************
View full article