Example S32K144 Flash RW simple

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example S32K144 Flash RW simple

Example S32K144 Flash RW simple

********************************************************************************
* Detailed Description:
* This simple example shows how to force function to RAM memory in S32 Design
* Studio and how to perform flash functions (Erase flash sector and Program
* phrase command in this case).
*
* ------------------------------------------------------------------------------
* Test HW:         FRDM-S32K144
* MCU:             PS32K144HFVLL 0N77P
* Fsys:            default
* Debugger:        Lauterbach Trace32
* Target:          internal_FLASH
*
********************************************************************************

Labels (1)
Attachments
Comments

You can explain FCCOB Number 1 -> number 2. How to determine to fill this field.

example i want write into last sector in Program flash. How to do it 

is there any documentation to understand the example?

In my application I want to write some date in to flash and read it back after a power cycle.

could you please point me to a specific example.

Kind regards

No ratings
Version history
Last update:
‎09-26-2016 01:27 AM
Updated by: