********************************************************************************
* Detailed Description:
* RAM self-test is performed after reset in startup_S32K144.s file.
* The RAM self-test should be executed right after reset, so it does not destroy
* data loaded to RAM by init functions. The code is inserted after
* initialization of core registers. RAM initialization is commented out because
* the same operation is done by the self-test.
* The test flow is:
* 1. Write pattern 0x55AA55AA to first word in RAM
* 2. Read the data back
* 3. Compare the data and increment error counter if not equal
* 4. Write inverse pattern 0xAA55AA55 to first word in RAM
* 5. Read the data back
* 6. Compare the data and increment error counter if not equal
* 7. Clear the first word in RAM to leave whole RAM erased to ‘0’ at the end of test
* This procedure is repeated for whole RAM.
* If the error counter is different from zero at the end, the program stays in
* endless loop until watchdog reset.
*
* ------------------------------------------------------------------------------
* Test HW: S32K144EVB-Q100
* MCU: FS32K144UAVLL 0N57U
* Fsys: Default
* Debugger: Lauterbach Trace32
* Target: internal_FLASH
*
********************************************************************************