S32G2-GoldVIP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32G2-GoldVIP

2,162件の閲覧回数
qifa
Contributor I

The GoldVIP-gateway project is loading missing components on EB

0 件の賞賛
返信
3 返答(返信)

2,139件の閲覧回数
nxf92355
NXP Employee
NXP Employee

Hi gao qifa ,

 

Hope you are doing well

 

You can link module with EB tresos during installation time of module.

As shown below you will be ask to Choose install location for EB tresos

Screenshot.pngScreenshot.png

Browse the EB path like C:\EB\tresos

installation will automatically link to EB tresos

 

Or another way is copy.

For missing modules you can copy module plugins to your EB Tresos Plugins Directory (C:\EB\tresos\plugins)

For GoldVIP 1.9.0 plugins

  • Extract GoldVIP-S32G2-1.9.0-binaries.zip
  • Go to \GoldVIP for S32G2 1.9.0\configuration\s32g274ardb2\can-gw\eclipse\plugins
  • Extract plugins.zip
  • Copy and paste it into C:\EB\tresos\plugins

 RTD 4.0.1 Plugins:

  • Run SW32G_RTD_4.4_4.0.1_D2302.exe
  • Find the folder under C:\NXP\SW32G_RTD_4.4_4.0.1_D2302
  • Copy module plugins C:\NXP\SW32G_RTD_4.4_<version>\eclipse\plugins to C:\EB\tresos\plugins

 Platform Software Integration 2023_06 Plugins

  • Run Platform_Software_Integration_S32G2_2023_06.exe
  • Perform the same procedure as above

 

Best Regards  ,

Tushar

0 件の賞賛
返信

2,096件の閲覧回数
qifa
Contributor I

qifa_0-1701314505501.jpegqifa_0-1701314505501.jpeg

We are currently importing the GoldVIP1.9 project into EB. All other modules can be opened, but the Platforms cannot be opened. Can you help solve this problem

0 件の賞賛
返信

2,085件の閲覧回数
nxf92355
NXP Employee
NXP Employee

Hi ,

is current issue solved ?

Please raise new ticket for new issue.

0 件の賞賛
返信