S32G2-GoldVIP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32G2-GoldVIP

2,260 次查看
qifa
Contributor I

The GoldVIP-gateway project is loading missing components on EB

0 项奖励
回复
3 回复数

2,237 次查看
nxf92355
NXP Employee
NXP Employee

Hi gao qifa ,

 

Hope you are doing well

 

You can link module with EB tresos during installation time of module.

As shown below you will be ask to Choose install location for EB tresos

Screenshot.png

Browse the EB path like C:\EB\tresos

installation will automatically link to EB tresos

 

Or another way is copy.

For missing modules you can copy module plugins to your EB Tresos Plugins Directory (C:\EB\tresos\plugins)

For GoldVIP 1.9.0 plugins

  • Extract GoldVIP-S32G2-1.9.0-binaries.zip
  • Go to \GoldVIP for S32G2 1.9.0\configuration\s32g274ardb2\can-gw\eclipse\plugins
  • Extract plugins.zip
  • Copy and paste it into C:\EB\tresos\plugins

 RTD 4.0.1 Plugins:

  • Run SW32G_RTD_4.4_4.0.1_D2302.exe
  • Find the folder under C:\NXP\SW32G_RTD_4.4_4.0.1_D2302
  • Copy module plugins C:\NXP\SW32G_RTD_4.4_<version>\eclipse\plugins to C:\EB\tresos\plugins

 Platform Software Integration 2023_06 Plugins

  • Run Platform_Software_Integration_S32G2_2023_06.exe
  • Perform the same procedure as above

 

Best Regards  ,

Tushar

0 项奖励
回复

2,194 次查看
qifa
Contributor I

qifa_0-1701314505501.jpeg

We are currently importing the GoldVIP1.9 project into EB. All other modules can be opened, but the Platforms cannot be opened. Can you help solve this problem

0 项奖励
回复

2,183 次查看
nxf92355
NXP Employee
NXP Employee

Hi ,

is current issue solved ?

Please raise new ticket for new issue.

0 项奖励
回复