S32G2-GoldVIP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G2-GoldVIP

2,350 Views
qifa
Contributor I

The GoldVIP-gateway project is loading missing components on EB

0 Kudos
Reply
3 Replies

2,327 Views
nxf92355
NXP Employee
NXP Employee

Hi gao qifa ,

 

Hope you are doing well

 

You can link module with EB tresos during installation time of module.

As shown below you will be ask to Choose install location for EB tresos

Screenshot.png

Browse the EB path like C:\EB\tresos

installation will automatically link to EB tresos

 

Or another way is copy.

For missing modules you can copy module plugins to your EB Tresos Plugins Directory (C:\EB\tresos\plugins)

For GoldVIP 1.9.0 plugins

  • Extract GoldVIP-S32G2-1.9.0-binaries.zip
  • Go to \GoldVIP for S32G2 1.9.0\configuration\s32g274ardb2\can-gw\eclipse\plugins
  • Extract plugins.zip
  • Copy and paste it into C:\EB\tresos\plugins

 RTD 4.0.1 Plugins:

  • Run SW32G_RTD_4.4_4.0.1_D2302.exe
  • Find the folder under C:\NXP\SW32G_RTD_4.4_4.0.1_D2302
  • Copy module plugins C:\NXP\SW32G_RTD_4.4_<version>\eclipse\plugins to C:\EB\tresos\plugins

 Platform Software Integration 2023_06 Plugins

  • Run Platform_Software_Integration_S32G2_2023_06.exe
  • Perform the same procedure as above

 

Best Regards  ,

Tushar

0 Kudos
Reply

2,284 Views
qifa
Contributor I

qifa_0-1701314505501.jpeg

We are currently importing the GoldVIP1.9 project into EB. All other modules can be opened, but the Platforms cannot be opened. Can you help solve this problem

0 Kudos
Reply

2,273 Views
nxf92355
NXP Employee
NXP Employee

Hi ,

is current issue solved ?

Please raise new ticket for new issue.

0 Kudos
Reply