S32G2 Ethernet PFE module is not getting initilialized

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32G2 Ethernet PFE module is not getting initilialized

3,881 次查看
Imsiya
Contributor I

Hello All, 

 

I am working on enable ethernet communication in our project. But Eth_43_PFE driver is not getting initialised. After debugging identified as if condition is not getting passed and partitionStat is not setting  to True. Please guide me to resolve this issue.

 

/**
* brief Checks the access to the controller
* details This function is intended to check whether the controller can be accessed or not by reading clock partition enable bit (partition 2 for PFE),
the field PCS. The capability to access the controller will be similar to the return value.
* return Controller accessibility
* retval TRUE Controller is accessible
* retval FALSE Controller access failed
*/
boolean Eth_PFE_LLD_CheckAccessToController(void)
{
boolean partitionStat = FALSE;

if(MC_ME_PRTN_STAT_PCS == (hal_read32(MC_ME_BASE + MC_ME_PRTN2_STAT) & MC_ME_PRTN_STAT_PCS))
{
partitionStat = TRUE;
}
return partitionStat;
}

 

0 项奖励
回复
12 回复数

3,864 次查看
Imsiya
Contributor I

Hello Daniel,

Thanks for your reply.

Yes, we are using NXP board. Currently we are using the RTD version 3.0.3.  Firware version is PFE-FW_S32G_RTM_1.3.0.

 

0 项奖励
回复

3,848 次查看
Imsiya
Contributor I

Hello Daniel,

The issue that I mentioned earlier has been resolved. The issue was related to MCU Clock Configuration. Now we are facing other error while trying to read the pfe version from pfe_platform_init. You can see the images. While trying to read the pfe version , bus fault exception is triggering from the Os. we are not using the core partition and we don't have a memory mapping in the linker script at the moment, as we are in the beginning stage of  the project. Is the issue is related to missing of proper memory mapping? you can see the screen shot from lauterbach  and tresos configuration below.

Request your support.

error3.PNGError1.PNGerror2.PNG

0 项奖励
回复

3,839 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for the information. We will provide this additional information to our internal team to confirm if the memory mapping inside the linker file is needed for this situation.

Please, let us know.

0 项奖励
回复

3,818 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We have received the following information from our internal team:

"I would suggest to check following steps before loading PFE driver

DanielAguirre_0-1682029799495.png

 

And then please suggest to follow PFE MCAL driver integration manual to complete PFE driver integration. It should be careful about PFE memory allocation which is descripted in Chapter 8."

Please, let us know.

0 项奖励
回复

3,728 次查看
Imsiya
Contributor I

Hello,

Thanks for the detail updates. Unfortunately, our issues are not resolved. Still Eth_43_PFE is not initialized. 

We are facing issues in MCU PFE Partition clock. Only PRTN_STAT0 Clock is active PRTN_STAT1 and PRTN_STAT2 are Inactive. Below the register value of PRTN2_STAT is zero. How can we set this to 1?

Eth_43_PFE_LLD_AccessControlCheck.PNG

We have done MCU configuration. Any Port configurations are required to enable these clocks? 

Partition Clock.png

Please see the tresos configuration below.

PartitionTresos.png

0 项奖励
回复

3,715 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

It is said on the S32G2 Reference Manual [Chapter 28.12.7, Page 1079, S32G2 Reference Manual, Rev. 6, 11/2022] that to enable the partition clocks, you should use the corresponding "MC_ME_PRTNn_PCONF[PCE]", is this being done inside the application? Image below:

DanielAguirre_0-1682368868451.png

Please, let us know.

0 项奖励
回复

3,590 次查看
Imsiya
Contributor I

Hello,

MC_ME_PRTNn_PCONF[PCE] for Partition 0 is enabling from CMM script. We don't have application SWC component to enable the partition clock at the moment. 

MC_ME_Partition0_CMM.PNG

 

We tried to enable the Partition 2 clock (MC_ME_PRTN2_PCONF) from the CMM as similar to Partition 0. But still the clock is not activated.

MC_ME_Partition2_CMM.PNG

 

Also we couldn't see the registers for enabling core 0 for partition 2 as similar for Partition 0. Could you please tell, can we enable the partition2 clock from the cmm ? If yes what is missing in our cmm?

0 项奖励
回复

3,569 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We have received the following comment from our internal team:

"can you provide the MCU configuration file(Mcu.xdm)?"

Given that this channel is a public one, we may recommend opening a ticket under the NXP online services, for a private channel.

Please, let us know.

0 项奖励
回复

3,562 次查看
Imsiya
Contributor I

Hello, 

We can provide the Mcu.xdm. Could you please share the link of NXP online services.

0 项奖励
回复

3,551 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

The NXP online service should be available under the "SUPPORT" tab inside the NXP home page (link: NXP® Semiconductors Official Site | NXP Semiconductors), as shown on the following image:

DanielAguirre_0-1683314855429.png

In there, you should be able to create a ticket and you should be able to provide this same community post link under the description, for future reference.

Please, let us know.

0 项奖励
回复

3,873 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Can you help us providing the following information?

  • Are you using an NXP board?
  • Which RTD version are you using?
  • Which PFE version are you using?

Please, let us know.

0 项奖励
回复

180 次查看
aaronbaranoff
Contributor III

What was the solution to this issue I have a similar problem. 

0 项奖励
回复