SystemInit api happens an error in S32K314

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SystemInit api happens an error in S32K314

Jump to solution
2,415 Views
HyunungPark1
Contributor III

I have any decoupled S32K344 (S32K314).

HardFault error happens SystemInit runs after the firmware is installed

MCAL version : SW32K3_RTD_4.4_R21-11_3.0.0_P01_HF02

Please find the attached file

/******************************************************************/
/* Autosar Guidance - In the start-up code a default */
/* initialization of the MCU clock system shall be performed */
/* including global clock prescalers. */
/******************************************************************/
__SYSTEM_INIT:
bl SystemInit

Could you please let me know for this issue?

 

Labels (1)
0 Kudos
Reply
1 Solution
2,387 Views
HyunungPark1
Contributor III

Hi Daniel.

This issue is resolved.

Thank you for your support.

Best Regards.

Hyunung Park

View solution in original post

0 Kudos
Reply
3 Replies
2,226 Views
jwkang
Contributor III
0 Kudos
Reply
2,397 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @HyunungPark1,

Seems like there is missing S32K314 macro for the MPU descriptor 2 in this 3.0.0 P01 revision.

danielmartynek_0-1702297129019.png

 

Regards,

Daniel

0 Kudos
Reply
2,388 Views
HyunungPark1
Contributor III

Hi Daniel.

This issue is resolved.

Thank you for your support.

Best Regards.

Hyunung Park

0 Kudos
Reply