Does the S32K344 have many STANDBY modes?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does the S32K344 have many STANDBY modes?

1,055件の閲覧回数
MNN
Contributor II

hello,
I want to put my S32K344 into STANDBY Mode, when I try to configure it on EB, I find that there are many modes of Operating Mode, but I only see that S32K344 has RUN and STANDBY modes in S32K344 RM. So I have a question, which one should I choose is the real STANDBY mode? What's the difference between these patterns? thank you.

MNN_0-1703685643580.png

 

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

993件の閲覧回数
CongDang
NXP Employee
NXP Employee

I think the information in UM will be helpful. I'm looking on UM of SW32K3_RTD_4.4_R21-11_3.0.0 - Chapter  3.6.5 How Mcu_SetMode works when entering Low Power mode

0 件の賞賛
返信