S32 DS for ARM for SDK RTM 4.0.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32 DS for ARM for SDK RTM 4.0.0

跳至解决方案
3,794 次查看
adria
Contributor I

Hello,

I am currently working with:

- SDK: RTM 3.0.0

- S32DS for ARM: 2018.R1

I want to upgrade SDK to RTM 4.0.0. I see in its release notes that it is compatible with S32DS 3.3, but it is not compatible with any version of S32DS for ARM. Also in the next link S32 Design Studio IDE for Arm® based MCUs | NXP I can see how the latest S32DS for ARM version is 2.2.

I work with both S32K146 and S32K116.

Would you recommend me to start working with S32DS and stop working with S32DS for ARM so I can start already using SDK RTM 4.0.0 or should I wait for a version of S32DS for ARM compatible with SDK RTM 4.0.0? In case the answer is that I should wait for an S32DS for ARM version compatible with SDK RTM 4.0.0, then when is the estimated date for such version to be released?

Thanks in advance!

Best regards,

Adria

标记 (2)
0 项奖励
回复
1 解答
3,697 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello Adria,

This question is more for S32DS support. Unfortunately, I cannot find any documents related to migration.

I have only found the "Migrate" option in the menu "File" of the S32DS 3.3.

Best regards,

Diana

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,697 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello Adria,

I have checked it and S32DS 3.3 already supports S32K devices and RTM 4.0.0, please, refer to link below:

https://community.nxp.com/docs/DOC-347212 

I believe it helps.

Best regards,

Diana

0 项奖励
回复
3,697 次查看
adria
Contributor I

Hello Diana,

It helped, thanks.

By the way, the link says: Migration support for projects created in S32DS for ARM v2.2 (with Processor Expert).

Is there also support for projects from 2018.R1?

And about this support, is it through a document, a tool or how?

Best regards,

Adria

0 项奖励
回复
3,698 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello Adria,

This question is more for S32DS support. Unfortunately, I cannot find any documents related to migration.

I have only found the "Migrate" option in the menu "File" of the S32DS 3.3.

Best regards,

Diana

0 项奖励
回复