s32d live expression for power pc debugging

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

s32d live expression for power pc debugging

ソリューションへジャンプ
3,879件の閲覧回数
InHome
Contributor III

Dear nxp Hello,

I am using sd32 for power pc dev and debugging. I have a problem with the watch expression.

However, I could not see the live expression. I couldn't modify a global variable using the expression window.

I ma using OpenSDA interface for debugging 

Thank you in advance

 

タグ(1)
0 件の賞賛
返信
1 解決策
3,763件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

the live expression is available only for ARM processors. 

 

Jiri 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,422件の閲覧回数
kyf
Contributor V

Hello.

I'm sorry for reopening this case. I'm looking for "live expression" tool for S32K344 MCU. Is this tool included in S32DS or I have to download an extra tool/plugin for it ?

I'm developing FW for S32K344 with

S32 Design Studio for S32 Platform
Version: 3.4
Build id: 201217 (Update 3)
Copyright 2017-2021 NXP

and I'm using DEV board: S32K3x4-Q172 General-Purpose Development Board 

 

 

Kind regards,

kyf

 

0 件の賞賛
返信
3,417件の閲覧回数
kyf
Contributor V

I've found the solution into this post: How do I enable Live View for variables when debugging?  !!!

0 件の賞賛
返信
3,764件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

the live expression is available only for ARM processors. 

 

Jiri 

0 件の賞賛
返信