s32d live expression for power pc debugging

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32d live expression for power pc debugging

Jump to solution
2,599 Views
InHome
Contributor III

Dear nxp Hello,

I am using sd32 for power pc dev and debugging. I have a problem with the watch expression.

However, I could not see the live expression. I couldn't modify a global variable using the expression window.

I ma using OpenSDA interface for debugging 

Thank you in advance

 

Tags (1)
0 Kudos
Reply
1 Solution
2,483 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

the live expression is available only for ARM processors. 

 

Jiri 

View solution in original post

0 Kudos
Reply
3 Replies
2,142 Views
kyf
Contributor V

Hello.

I'm sorry for reopening this case. I'm looking for "live expression" tool for S32K344 MCU. Is this tool included in S32DS or I have to download an extra tool/plugin for it ?

I'm developing FW for S32K344 with

S32 Design Studio for S32 Platform
Version: 3.4
Build id: 201217 (Update 3)
Copyright 2017-2021 NXP

and I'm using DEV board: S32K3x4-Q172 General-Purpose Development Board 

 

 

Kind regards,

kyf

 

0 Kudos
Reply
2,137 Views
kyf
Contributor V

I've found the solution into this post: How do I enable Live View for variables when debugging?  !!!

0 Kudos
Reply
2,484 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

the live expression is available only for ARM processors. 

 

Jiri 

0 Kudos
Reply