What the maximum size of DDR RAM can be installed on S32V234EVB?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What the maximum size of DDR RAM can be installed on S32V234EVB?

2,091件の閲覧回数
antonvoloshchuk
Contributor I

What the maximum size of DDR RAM can be installed on S32V234EVB: 2/4 Gbytes, maybe more?

タグ(3)
0 件の賞賛
返信
2 返答(返信)

1,964件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi Anton,

As far as I know DDR memory cannot be extended since they are populated directly on S32V234EVB.

There 2 x 2Gbit DDR chips.

Stan

1,964件の閲覧回数
antonvoloshchuk
Contributor I

Thanks for answer.

0 件の賞賛
返信