What the maximum size of DDR RAM can be installed on S32V234EVB?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What the maximum size of DDR RAM can be installed on S32V234EVB?

2,087 Views
antonvoloshchuk
Contributor I

What the maximum size of DDR RAM can be installed on S32V234EVB: 2/4 Gbytes, maybe more?

Tags (3)
0 Kudos
Reply
2 Replies

1,960 Views
stanish
NXP Employee
NXP Employee

Hi Anton,

As far as I know DDR memory cannot be extended since they are populated directly on S32V234EVB.

There 2 x 2Gbit DDR chips.

Stan

1,960 Views
antonvoloshchuk
Contributor I

Thanks for answer.

0 Kudos
Reply