What are the various error parsers for?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What are the various error parsers for?

ソリューションへジャンプ
1,938件の閲覧回数
dj_hacker
Contributor I

There are a lot of error parsers available in S32 Design Studio projects. Based on their names, I know what tools some of them parse, but there are a few I'm not familiar with. Can somebody please tell me what tools and/or products the following error parsers apply to?

Freescale COBJ Error Parser (what is COBJ?)

Freescale ICODE Error Parser (what is ICODE?)

Freescale LLT Error Parser (what is LLT?)

MPW Error Parser (what is MPW?)

Freescale Fsscc Error Parser (what is Fsscc?)

Thanks!

 

ラベル(1)
0 件の賞賛
返信
1 解決策
1,909件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello @dj_hacker,

These are legacy parsers which were reused from a previous product. They were intended to extend the default parser for particular tools which are designed to catch rare error expressions. Some of them may, in fact, be redundant. We might review them sometime in the future and determine if they are still needed, but it is a low priority at this time.

Hope that helps,

Mike

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,910件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello @dj_hacker,

These are legacy parsers which were reused from a previous product. They were intended to extend the default parser for particular tools which are designed to catch rare error expressions. Some of them may, in fact, be redundant. We might review them sometime in the future and determine if they are still needed, but it is a low priority at this time.

Hope that helps,

Mike

0 件の賞賛
返信