What are the various error parsers for?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What are the various error parsers for?

Jump to solution
1,920 Views
dj_hacker
Contributor I

There are a lot of error parsers available in S32 Design Studio projects. Based on their names, I know what tools some of them parse, but there are a few I'm not familiar with. Can somebody please tell me what tools and/or products the following error parsers apply to?

Freescale COBJ Error Parser (what is COBJ?)

Freescale ICODE Error Parser (what is ICODE?)

Freescale LLT Error Parser (what is LLT?)

MPW Error Parser (what is MPW?)

Freescale Fsscc Error Parser (what is Fsscc?)

Thanks!

 

Labels (1)
0 Kudos
Reply
1 Solution
1,891 Views
mikedoidge
NXP Employee
NXP Employee

Hello @dj_hacker,

These are legacy parsers which were reused from a previous product. They were intended to extend the default parser for particular tools which are designed to catch rare error expressions. Some of them may, in fact, be redundant. We might review them sometime in the future and determine if they are still needed, but it is a low priority at this time.

Hope that helps,

Mike

View solution in original post

0 Kudos
Reply
1 Reply
1,892 Views
mikedoidge
NXP Employee
NXP Employee

Hello @dj_hacker,

These are legacy parsers which were reused from a previous product. They were intended to extend the default parser for particular tools which are designed to catch rare error expressions. Some of them may, in fact, be redundant. We might review them sometime in the future and determine if they are still needed, but it is a low priority at this time.

Hope that helps,

Mike

0 Kudos
Reply