Unable to find SCB in EmbSys Registers

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Unable to find SCB in EmbSys Registers

跳至解决方案
1,245 次查看
Janeting123
Contributor I

I encountered the same problem as this post.

https://community.nxp.com/t5/S32-Design-Studio/these-is-no-SCB-registers-in-peripheral-registers-vie...

Snipaste_2024-05-13_16-50-28.png

The S32DS version I am using is 3.4. The installed extensions are as followsSnipaste_2024-05-13_16-33-58.png

 

0 项奖励
回复
1 解答
1,204 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @Janeting123 

To view the information in the Peripheral Registry view is necessary to start a debug session. Could you check if you can see the information when debugging any example code?

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,230 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @Janeting123 

I tested it with S32DS v3.4 and S32K3XX RTD v2.0.1 and there is no issue. Please instead of using the EmbSys Registers view use the Peripherals Registers view. 

VaneB_1-1715631148899.png

Additionally, the S32K3XX RTD v4.0.0 P20 was developed and tested with S32DS v3.5, so, its functionality is not guaranteed in older IDE versions.

 

B.R.

VaneB

 

0 项奖励
回复
1,217 次查看
Janeting123
Contributor I

This is my peripheral register and it is emptySnipaste_2024-05-14_09-54-25.png

0 项奖励
回复
1,205 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @Janeting123 

To view the information in the Peripheral Registry view is necessary to start a debug session. Could you check if you can see the information when debugging any example code?

0 项奖励
回复