Unable to configure the peripherals using "ConfigTool" option in the S32 Design Studio IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to configure the peripherals using "ConfigTool" option in the S32 Design Studio IDE

Jump to solution
3,727 Views
Anilpatil_SasvaAuto
Contributor III

Hello Team,

I am trying to configure the peripherals using the "ConfigTool" provided in the S32 Design Studio IDE. However, I'm encountering errors and am unable to complete the configuration.

Could you please check and let me know why these errors are occurring? I would appreciate it if you could provide a solution. I have attached the relevant files for your reference. Thank you!

0 Kudos
Reply
1 Solution
3,465 Views
Anilpatil_SasvaAuto
Contributor III
0 Kudos
Reply
13 Replies
3,474 Views
Anilpatil_SasvaAuto
Contributor III

Please provide the solution

0 Kudos
Reply
3,467 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Please show me a screenshot of the error.

Some companies' IT restricts http access, Did you change Available S32DS Software Sites to https

0 Kudos
Reply
3,719 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Seems that you want to import the S32K1 SDK 4.0.3 based project. 

Please install S32DS v3.4 + S32K1 SDK 4.0.3 by refer to the discussion in Where can I find it?S32_SDK_S32K1xx_RTM_4.0.3

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
3,693 Views
Anilpatil_SasvaAuto
Contributor III
I am not able to find the "S32K1 SDK 4.0.3" and install
0 Kudos
Reply
3,679 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

The S32 SDK for S32K1xx RTM 4.0.3 should be listed in Extensions and Updates

0 Kudos
Reply
3,606 Views
Anilpatil_SasvaAuto
Contributor III
Unable to install, getting error
0 Kudos
Reply
3,582 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Please show me a screenshot of the error.

Some companies' IT restricts http access, Did you change Available S32DS Software Sites to https

0 Kudos
Reply
3,466 Views
Anilpatil_SasvaAuto
Contributor III

Please find the error details as attached

Screenshot 2025-05-30 160344.png

0 Kudos
Reply
3,460 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Please check if the S32K1xx development package has been installed?
If not, please install the S32K1xx development package first. Refer to:
 S32 Design Studio 3.4 S32K1xx Service Pack 1 (SW32K1_S32DS_3.4.1_D2106.zip) 

0 Kudos
Reply
3,453 Views
Anilpatil_SasvaAuto
Contributor III

I have changed to http but no use still same issue

0 Kudos
Reply
3,440 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Do not change it to http.   Please change it to https!

Did you install S32K1xx development package by refer to https://community.nxp.com/t5/S32K/Trying-to-install-the-S32SDK-S32K1xx-RTM-4-0-2-SDK-extension/td-p/... ?

S32K1xx development package.png

After you have installed SW32K1_S32DS_3.4.1_D2106.zip offline, you should be able to install S32SDK S32K1XX RTM 4.0.3 online via S32DS Extensions and Updates.

0 Kudos
Reply
3,196 Views
Anilpatil_SasvaAuto
Contributor III
Thanks, installed successfully
0 Kudos
Reply
3,466 Views
Anilpatil_SasvaAuto
Contributor III

FYI

0 Kudos
Reply