Unable to configure the peripherals using "ConfigTool" option in the S32 Design Studio IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to configure the peripherals using "ConfigTool" option in the S32 Design Studio IDE

ソリューションへジャンプ
3,160件の閲覧回数
Anilpatil_SasvaAuto
Contributor III

Hello Team,

I am trying to configure the peripherals using the "ConfigTool" provided in the S32 Design Studio IDE. However, I'm encountering errors and am unable to complete the configuration.

Could you please check and let me know why these errors are occurring? I would appreciate it if you could provide a solution. I have attached the relevant files for your reference. Thank you!

0 件の賞賛
返信
1 解決策
2,898件の閲覧回数
Anilpatil_SasvaAuto
Contributor III
0 件の賞賛
返信
13 返答(返信)
2,907件の閲覧回数
Anilpatil_SasvaAuto
Contributor III

Please provide the solution

0 件の賞賛
返信
2,900件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Please show me a screenshot of the error.

Some companies' IT restricts http access, Did you change Available S32DS Software Sites to https

0 件の賞賛
返信
3,152件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Seems that you want to import the S32K1 SDK 4.0.3 based project. 

Please install S32DS v3.4 + S32K1 SDK 4.0.3 by refer to the discussion in Where can I find it?S32_SDK_S32K1xx_RTM_4.0.3

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
3,126件の閲覧回数
Anilpatil_SasvaAuto
Contributor III
I am not able to find the "S32K1 SDK 4.0.3" and install
0 件の賞賛
返信
3,112件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

The S32 SDK for S32K1xx RTM 4.0.3 should be listed in Extensions and Updates

0 件の賞賛
返信
3,039件の閲覧回数
Anilpatil_SasvaAuto
Contributor III
Unable to install, getting error
0 件の賞賛
返信
3,015件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Please show me a screenshot of the error.

Some companies' IT restricts http access, Did you change Available S32DS Software Sites to https

0 件の賞賛
返信
2,899件の閲覧回数
Anilpatil_SasvaAuto
Contributor III

Please find the error details as attached

Screenshot 2025-05-30 160344.png

0 件の賞賛
返信
2,893件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Please check if the S32K1xx development package has been installed?
If not, please install the S32K1xx development package first. Refer to:
 S32 Design Studio 3.4 S32K1xx Service Pack 1 (SW32K1_S32DS_3.4.1_D2106.zip) 

0 件の賞賛
返信
2,886件の閲覧回数
Anilpatil_SasvaAuto
Contributor III

I have changed to http but no use still same issue

0 件の賞賛
返信
2,873件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Do not change it to http.   Please change it to https!

Did you install S32K1xx development package by refer to https://community.nxp.com/t5/S32K/Trying-to-install-the-S32SDK-S32K1xx-RTM-4-0-2-SDK-extension/td-p/... ?

S32K1xx development package.png

After you have installed SW32K1_S32DS_3.4.1_D2106.zip offline, you should be able to install S32SDK S32K1XX RTM 4.0.3 online via S32DS Extensions and Updates.

0 件の賞賛
返信
2,629件の閲覧回数
Anilpatil_SasvaAuto
Contributor III
Thanks, installed successfully
0 件の賞賛
返信
2,899件の閲覧回数
Anilpatil_SasvaAuto
Contributor III

FYI

0 件の賞賛
返信