S32DS 2.1 How to extend license

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32DS 2.1 How to extend license

跳至解决方案
3,044 次查看
kuhruhm
Contributor II

kuhruhm_0-1696623755930.png

How to extend(or renew) the S32DS license? I tried to re-install it. but I was halted on licensing.

0 项奖励
回复
1 解答
2,989 次查看
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @kuhruhm , 

 

I see the problem was because the older licenses was not returned. 

 

It should be fixed now. 

 

Please can you try installing now using the license. 

 

Thank you. Best regards. 

 

-Mehul Patel

在原帖中查看解决方案

0 项奖励
回复
6 回复数
3,034 次查看
kuhruhm
Contributor II

My S32DS is version 2.1

I tried to install it on a new computer.

Halted online licensing and I did stop by the task manager.

c:\NXP\S32DS_Power_v2.1\_S32 Design Studio for Power Architecture Version 2.1_installation\Logs\

Has no file.

0 项奖励
回复
3,026 次查看
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @kuhruhm , 

 

As I see in the below error in your log I think the issue is because of not running as administrator mode or not having enough permission while installation. 

Mehul_Patel_NXP_0-1696625746446.png

 

Your Windows user account must be a member of the administrator's group as mentioned in installation guide. https://www.nxp.com/docs/en/user-guide/S32DSPAIG.pdf 

The 'Run as Administrator' option should not be used for the installation of the S32 Design Studio. If you are getting an error on Windows permissions, then you likely do not have the necessary permissions to install.

Mehul_Patel_NXP_1-1696626152479.png

 

If you have issue to run as administrator mode please contact your IT department to for their assistance.

 

Please let us know if you are able to move further. 

 

Thank you. Best regards.

 

- Mehul Patel

 

 

 

0 项奖励
回复
2,999 次查看
kuhruhm
Contributor II

I retried as an administrator. but nothing changed.

but halted online licensing, and no log was created.

My license exp. is Oct 1, 2023

Entitlement Exp is Oct 3, 2027

Does this mean my license is active?

0 项奖励
回复
2,990 次查看
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @kuhruhm , 

 

I see the problem was because the older licenses was not returned. 

 

It should be fixed now. 

 

Please can you try installing now using the license. 

 

Thank you. Best regards. 

 

-Mehul Patel

0 项奖励
回复
2,984 次查看
kuhruhm
Contributor II

Yes, It works.

But when I clicked the return button, that did not work.

Problem solved, installation succeed.

Thank you.

0 项奖励
回复
3,041 次查看
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @kuhruhm , 

 

Please can you share the S32DS installation log from the : 

 

C:\NXP\S32DS.3.5\_S32 Design Studio for S32 Platform 3.5_installation\Logs

 

Thank you. 

 

Best regards. 

 

- Mehul Patel 

0 项奖励
回复