Project paths broken after update?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Project paths broken after update?

2,085件の閲覧回数
gearhead1107
Contributor IV


Hey folks, after I downloaded the most recent updates this morning, S32 design studio is throwing out *loads*of errors from parameters that should be in the middleware. There are two warnings showing that two paths are invalid:

DescriptionResourcePathLocationType
Invalid project path: Include path not found (\middleware\sbc\include).[project]pathentryPath Entry Problem
Invalid project path: Missing project folder or file: \[project]\S32K144_SDK_gcc for Source path.[project]pathentryPath Entry Problem

 

I've replaced the project title to "[project]" to keep our IP out of the public domain, but someone point me to how to fix these paths in the compiler settings?

 

Thanks, Andrew

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,789件の閲覧回数
raresvasile
NXP Employee
NXP Employee

Hi,

Can you go to Project Properties -> Resource -> Linked resource and provide me screenshots with the Path Variables and Linked Resources tabs?

Thank you,

Rares

0 件の賞賛
返信