Dose S32DS for Power V1.1 release?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Dose S32DS for Power V1.1 release?

ソリューションへジャンプ
3,027件の閲覧回数
enwei
NXP Employee
NXP Employee

Hi,

 

Question as the title, if yes, where can I download it? if not, what's the V 1.1 launch/release schdule?

 

PS: I found some bugs in S32DS for Power V1.0, and it's expected to be fixed in new released version.

 

Enwei Hu

ラベル(1)
タグ(1)
1 解決策
2,803件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hi,

S32DS for Power v 1.1 is not officially released yet (only some test builds), but it should be available at the end of Jun.

Regards,

Martin

元の投稿で解決策を見る

2 返答(返信)
2,804件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hi,

S32DS for Power v 1.1 is not officially released yet (only some test builds), but it should be available at the end of Jun.

Regards,

Martin

2,803件の閲覧回数
enwei
NXP Employee
NXP Employee

thank for your information, hope it will have big improvement~!

0 件の賞賛
返信