Project paths broken after update?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Project paths broken after update?

2,145 Views
gearhead1107
Contributor IV


Hey folks, after I downloaded the most recent updates this morning, S32 design studio is throwing out *loads*of errors from parameters that should be in the middleware. There are two warnings showing that two paths are invalid:

DescriptionResourcePathLocationType
Invalid project path: Include path not found (\middleware\sbc\include).[project]pathentryPath Entry Problem
Invalid project path: Missing project folder or file: \[project]\S32K144_SDK_gcc for Source path.[project]pathentryPath Entry Problem

 

I've replaced the project title to "[project]" to keep our IP out of the public domain, but someone point me to how to fix these paths in the compiler settings?

 

Thanks, Andrew

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,849 Views
raresvasile
NXP Employee
NXP Employee

Hi,

Can you go to Project Properties -> Resource -> Linked resource and provide me screenshots with the Path Variables and Linked Resources tabs?

Thank you,

Rares

0 Kudos
Reply