Processor S32K344, PlatformSDK_S32K3_2022_03 version is not supported by current version of the tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Processor S32K344, PlatformSDK_S32K3_2022_03 version is not supported by current version of the tool

1,613 Views
ars05
Contributor I

I am following the steps to test the software MR_CANHUBK3_IEEE1722 from the Getting Started with MR-CANHUBK344 Evaluation Board guide. I'm working with S32 Design Studio version 3.4 

In section 4.2, S32 Pin Tool, it instructs to right-click on “MR_CANHUBK3_IEEE1722” in the project explorer, then select S32 Configuration Tools → Open Pins. Once in the S32 Pin tool view, I click 'Update Code' and confirm with 'OK,' expecting the driver configuration files to generate.

However, I encounter the following error: Error during opening configuration FreeRTOS_Toggle_Led_Example_S32K344.mex: Processor S32K344, PlatformSDK_S32K3_2022_03 version is not supported by current version of the tool.

ars05_0-1731453178353.png

Could anyone advise on how to resolve this error?

0 Kudos
Reply
3 Replies

1,587 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

The MR_CANHUBK3_IEEE1722 project is created based on S32K3 Real Time Drivers Version 2.0.0.
Please try Offline Package Installation Setup:
SW32K3_S32DS_3.4.3_D2112.zip  SW32K3_S32DS_3.4.3_D2205.zip
SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204.zip

It is recommended to take a look at the installation method mentioned here: S32K3 Unified Bootloader Build Issue


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,570 Views
ars05
Contributor I

Versions SW32K3_S32DS_3.4.3_D2112.zip  SW32K3_S32DS_3.4.3_D2205.zip are not available: 

ars05_0-1731513016171.png

 

0 Kudos
Reply

1,546 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Sorry for the inconvenience we bring you! 
I didn't notice that SW32K3_S32DS_3.4.3_D2112.zip SW32K3_S32DS_3.4.3_D2205.zip are no longer available for customers who haven't downloaded them previously.
Please download SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204.zip and add it to S32DS Extensions and Updates.(refer to HOWTO: S32 Design Studio - Offline Install of Extensions and Updates) S32DS Extensions and Updates should then be able to install SW32K3_S32DS_3.4.3_D2205.zip as well.

0 Kudos
Reply